iMX6Q not detecting in serial download mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q not detecting in serial download mode

1,196 次查看
riteshpatel
Contributor II

Hi, 

I have two boards which are not detecting in USB serial download mode to flash U-boot and Kernal image.

All power to the processor is working fine. Reset sequence is proper and Reset logic state is High after power up.

The Boot mode selection pin settings are proper with proper logic level.

Is there any way to debug using JTAG interface? We have JTAG interface on our board. If yes, can you suggest the connection and required JTAG debugger tool?

Any other suggestions would be greatly appreciated.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

996 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes you can use Jtag, more detailed information, pls refer to the link as below:

https://community.nxp.com/message/953055?commentID=953055#comment-953055

0 项奖励
回复