iMX6Q: Yocto mini-image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q: Yocto mini-image

Jump to solution
3,788 Views
Tarek
Senior Contributor I

Hi,

What is the smallest minimum image to bitbake in Yocto that provides GStreamer and HW acceleration with no GUI nor X ?

Also is BSP 4.0.0 full integrated now in the dylan branch? if not when is it expected to be released and in which branch?

Thanks

Labels (4)
1 Solution
2,488 Views
LeonardoSandova
Specialist I

There are three Freescale Images,

$ bitbake-layers show-recipes | grep image | grep fsl

Parsing recipes..done.

fsl-image-gui:

fsl-image-gui-sdk:

fsl-image-test:

And the smallest you can get with GSTreamer FSL plugins is fsl-image-test

$ cat ../sources/meta-fsl-demos/recipes-fsl/images/fsl-image-test.bb

include recipes-core/images/core-image-base.bb

IMAGE_FEATURES += "debug-tweaks"

SOC_EXTRA_IMAGE_FEATURES ?= "tools-testapps"

# Add extra image features

EXTRA_IMAGE_FEATURES += " \

    ${SOC_EXTRA_IMAGE_FEATURES} \

    nfs-server \

    tools-debug \

    tools-profile \

"

IMAGE_INSTALL += " \

    packagegroup-fsl-gstreamer \

    packagegroup-fsl-tools-testapps \

    packagegroup-fsl-tools-benchmark \

"

export IMAGE_BASENAME = "fsl-image-test"


View solution in original post

0 Kudos
Reply
4 Replies
2,488 Views
OtavioSalvador
Senior Contributor II

The BSP 4.0 is available, in community BSP, only in master branch.

We're maintaining a set of custom BSPs for customers (at O.S. Systems) with this ported to dylan.

2,488 Views
Tarek
Senior Contributor I

I'm not interested in the GPU drivers. All I need is the latest MM codecs and Gstreamer as well as the the latest kernel fixes.

Which branch shall I use, Master or dylan ?

Thanks

0 Kudos
Reply
2,488 Views
OtavioSalvador
Senior Contributor II

The 3.0.7 MM codec is in master (of community). For use dylan with it, you'll need to maintain a backport or use one vendor to do it for you.

0 Kudos
Reply
2,489 Views
LeonardoSandova
Specialist I

There are three Freescale Images,

$ bitbake-layers show-recipes | grep image | grep fsl

Parsing recipes..done.

fsl-image-gui:

fsl-image-gui-sdk:

fsl-image-test:

And the smallest you can get with GSTreamer FSL plugins is fsl-image-test

$ cat ../sources/meta-fsl-demos/recipes-fsl/images/fsl-image-test.bb

include recipes-core/images/core-image-base.bb

IMAGE_FEATURES += "debug-tweaks"

SOC_EXTRA_IMAGE_FEATURES ?= "tools-testapps"

# Add extra image features

EXTRA_IMAGE_FEATURES += " \

    ${SOC_EXTRA_IMAGE_FEATURES} \

    nfs-server \

    tools-debug \

    tools-profile \

"

IMAGE_INSTALL += " \

    packagegroup-fsl-gstreamer \

    packagegroup-fsl-tools-testapps \

    packagegroup-fsl-tools-benchmark \

"

export IMAGE_BASENAME = "fsl-image-test"


0 Kudos
Reply