iMX6Q: Windows iotcore USB device support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q: Windows iotcore USB device support

3,159件の閲覧回数
Zaid_Noordeen
Contributor II

Hey there,
I found a UFX Chipidea interface identifier in the Dsdt-Usb.asl file of windows 10 iotcore, running on iMX6Q. Will this work in USB device mode? Any reference logs for the same will be helpful.
Thanks

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,147件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Zaid,

It will work under the USB, but the USB does not have the specific driver for ChipIdea, I guess will be supported limited or you have to develop your own driver.

 

Regards

 

0 件の賞賛
返信

3,123件の閲覧回数
Zaid_Noordeen
Contributor II

Hi,

     I've modified the Dsdt-Usb.asl file. Please find the modified file attached and verify if its correct. Are there any other modifications to be done to make the board to work as a USB device?

PS: The modifications are in line number 86 and 97 where by default, the functions which were returning 1(Host) are now made to return 0(Device). After these modifications, the board stopped detecting USB devices such as mouse, keyboard etc. 

0 件の賞賛
返信