iMX6Q Target Description File for GDB 4.7.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q Target Description File for GDB 4.7.3

1,159 Views
MikeJones
Contributor III

I need to know what Target Description File to use for GDB 4.7.3. I have tried arm-with-neon.xml from https://sourceware.org/git/gitweb.cgi?p=binutils-gdb.git;a=tree;f=gdb/features;hb=HEAD but I get errors when GDB reads FP registers and the CPSR is not correct.

Does anybody know which file is correct? And what file do I use if NEON is disabled?

If there are some issues with what has to be enabled by code for it to work, please express the answer in terms of the SDK, as that is the code I am using.

Labels (2)
0 Kudos
Reply
0 Replies