iMX6Q SSI slave mode timing specifications

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q SSI slave mode timing specifications

1,261 次查看
ThierryH_
Contributor I

Hi,

We are using SSI in I2S slave mode with 24 bits audio sample . Sample frequency is  48KHz up to 192KHz.

Into the "i.MX 6Dual/6Quad Applications Processors for Industrial Products, Rev. 4, 07/2015", chap 4.11.19.3 SSI Transmitter Timing with External Clock mention :

AUDx_TXC (Input), timing SS22 = 81.4ns min (12.285.. MHz max)

I2S slave = 2 time slot of 32 bits = 64 bits per frame =

  •  @48KHz : 48000*2*32 = 3.072MHz
  • @192KHz : 192000*2*32 = 12.288MHz

Does it means that @192KHz I2S 32bits shouldn't work correctly...?

Thanks

标签 (2)
0 项奖励
回复
1 回复

1,139 次查看
art
NXP Employee
NXP Employee

The i.MX6Q SSI module does not support 32-bit wide samples. The maximum sample width supported is 24 bits.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复