iMX6DQ IPU CPMEM Bus Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DQ IPU CPMEM Bus Address

1,622件の閲覧回数
ogj
Contributor IV

I'd like to know the bus address for the CPMEM for ipu1 and ipu2 in the iMX6Q. According to the RM, ipu1 is at 0x0260_0000 and ipu2 is at 0x02A0_0000. It appears from the SDK that the CPMEM is at the ipu base address + 0x0010_0000, but I'd like to make sure.

Another thing that puzzles me is the the RM shows the structure of the CPMEM as 80 channels x 2 mega-words per channel; each mega-word being 160-bits (5x 32-bit words).

ogj_0-1602620976807.png

The SDK structs for the CPMEM are:


struct ipu_cpmem_word
{
uint32_t data[5];
uint32_t res[3];
};

typedef struct ipu_cpmem
{
struct ipu_cpmem_word word[2];
} ipu_cpmem_t;

in the ipu_common.h file. I don't understand what the res[3] is for after each 160-bit mega-word.

 

iMX6 SDK shows the structure of

0 件の賞賛
返信
2 返答(返信)

1,609件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ogj

 

>appears from the SDK that the CPMEM is at the ipu base address + 0x0010_0000,

>but I'd like to make sure.

 

correct

 

>I don't understand what the res[3] is for after each 160-bit mega-word.

 

one can refer to (Word 1) Table 37-14. Channel Parameters Memory

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

Best regards
igor

 

 

 

0 件の賞賛
返信

1,603件の閲覧回数
ogj
Contributor IV

Found the answer in Section 37.4.2.10.2 of the RM. Although each mega-word is 160 bits (5x 32-bit words), each word has to start on a 256-bit boundary (8x 32-bit words).

Thanks for your quick response.

0 件の賞賛
返信