iMX6DL Windows 10 IOT USB not detecting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DL Windows 10 IOT USB not detecting

10,037件の閲覧回数
inayathraza
Contributor I

We download the source code from the link

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=W1809_1_1_0_imx-iotcore&appType=file1&DO...

and build the default FFU and Flashed it into SD and booted the imx6dl, But USB is not Detecting, we tried keyboard, as well as pen drives, But as per NXP Documentation USB host support, which is available in the BSP

Why we are not able to connect USB devices to the Board?

We tried with Default NXP images also we are facing the same issue with that images too

0 件の賞賛
返信
11 返答(返信)

9,851件の閲覧回数
m_syed_ahmed
Contributor III

Hi Igor,

I am working with Inayath. In Linux Demo Image, USB Host is working fine for us but in Windows IOT image, its not working as it is. Logs for Windows IOT boot and Linux boot is attached in previous message. 

In Windows IOT, LVDS display is getting up, but we are not able to get any relevant logs in debug port. Also USB Host and touch is not working means, we were not able to verify other drivers.

0 件の賞賛
返信

9,839件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m_syed_ahmed

 

had you tried to connect usb stick as suggested, with usb_id low.

Low level configures usb driver as host.

 

Best regards
igor

0 件の賞賛
返信

9,813件の閲覧回数
m_syed_ahmed
Contributor III

Hi Igor,

Thanks for your comments. Can I assume that by default, NXP image won't detect USB Host and we needs to modify in BSP to make USB host to work?

0 件の賞賛
返信

9,800件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m_syed_ahmed

 

> Can I assume that by default, NXP image won't detect USB Host and
>we needs to modify in BSP to make USB host to work?
 
it is enabled by default, no need to modify BSP.

 

Best regards
igor

0 件の賞賛
返信

9,775件の閲覧回数
m_syed_ahmed
Contributor III

Hi Igor,

Thanks for your support. Our USB OTG cable was not functioning, we changed that and USB Host is working fine. 

Additionally, I needs to know pin muxing for Windows IOT will only be done in UBoot or we needs to do the same in GPIO driver also.

0 件の賞賛
返信

10,016件の閲覧回数
inayathraza
Contributor I

Hi igor, Thanks for Reply

 

I am working on the IMX6DL sabresd board, Is there any way to enable USB, in Release Note its, mentioned as the USB stack is not enabled in
UEFI by default, How we can enable this in our FFU?

0 件の賞賛
返信

9,861件の閲覧回数
inayathraza
Contributor I

We are using MCIMX6DL-SDP 700-27417 REV C SCH-27417 REV C4 Sabre_iMX6DL_1GB board,

the same board is mentioned in release notes

0 件の賞賛
返信

9,855件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

are you able to see below (from p.61 i.MX Windows 10 IoT Core User’s Guide​)

 

1.jpg

 

 

 

for connection usb stick to usb otg, signal usb_id (pin4 J505 SPF-27417) should be low.

 

Best regards
igor

0 件の賞賛
返信

9,861件の閲覧回数
inayathraza
Contributor I

Hi Igor,

we are getting these log when we flashed default images from NXP website.

In the Same board when we are using Linux images USB host is working

0 件の賞賛
返信

8,849件の閲覧回数
scott3303
Contributor II

Hello,

Can you share the way to enable debug over serial from uefi.fit?

Thanks in advance,

Tommaso

0 件の賞賛
返信

10,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi inayathraza

 

reason may be that usb interface on custom board is not working. One

can check 24MHz crystal using IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

voltage on VDDUSB_CAP, try to perform usb test

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/I-MX6-series-USB-Certification-Guides/ta...

 

Best regards
igor

0 件の賞賛
返信