iMX6 to RGMII communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 to RGMII communication

1,351 Views
mylsamy_m
Contributor I

Hi,

Regarding iMX6 to RGMII communication we are using ENET_MDC and ENET_MDIO lines.

ENET_MDIO- This one is an bidirectional we have 4.7K pull up.

in which ENET_MDC is an clock output from iMX6 to Ethernet. Do we need any pull up resistor for MDC line?

Thanks and Regards

Labels (1)
0 Kudos
Reply
1 Reply

1,269 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mylsamy 

pull up is not required on MDC.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply