iMX6 solo flashing problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 solo flashing problem

1,059 Views
pyadvichuk
Contributor I

Hi all,

we have our custom board based on mx6sabreauto design with custom peripherals set. Previously we were using quad and dual cores imx6 CPUs on the same PCB without any modification and were able to get a stable production system based on yocto warrior BSP (4.19.35 kernel).

Now we're bringing up imx6 solo cpu on the same PCB and got stacked on the manufacturing stage. I was able to build mfgtools version of u-boot, kernel, DTB and initramfs but it seems something is missed in the commands execution flow. It looks like:

- u-boot is starting fine, cmdline for kernel is

console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idV
endor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused

- during kernel startup I see a crash in the main loop of USB gadget framework

 

g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
Unable to handle kernel NULL pointer dereference at virtual address 00000050
pgd = (ptrval)
[00000050] *pgd=00000000
Internal error: Oops: 817 [#1] PREEMPT SMP ARM
Modules linked in:
CPU: 0 PID: 92 Comm: file-storage Not tainted 4.19.35 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
PC is at fsg_main_thread+0x186c/0x21f8
LR is at _raw_spin_unlock_irqrestore+0x28/0x54
pc : [<80685ef4>]    lr : [<80a5fe30>]    psr: 600e0113
sp : 86623f08  ip : 00000000  fp : 8661ae00
r10: 43425355  r9 : 53425355  r8 : 86622000
r7 : 8642af00  r6 : 8661ae00  r5 : 00000000  r4 : 00000000
r3 : ffffffff  r2 : 00000009  r1 : 00000001  r0 : 8661ae00
Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment none
Control: 10c53c7d  Table: 16600059  DAC: 00000051
Process file-storage (pid: 92, stack limit = 0x(ptrval))
Stack: (0x86623f08 to 0x86624000)
3f00:                   00000000 8bb24180 86419e00 8661ae28 81004d08 81004e98
3f20: 00000000 00000000 8bb24180 80a5b480 00055302 a08f1000 00000000 80a5b958
3f40: 86614580 80a5b5e8 8603db1c 48412166 8641a270 600e0013 ffffe000 48412166
3f60: 866145dc 866145c0 86614580 00000000 86622000 8661ae00 80684688 8603db1c
3f80: 866145dc 8014bb1c 00000000 86614580 8014b9d4 00000000 00000000 00000000
3fa0: 00000000 00000000 00000000 801010e8 00000000 00000000 00000000 00000000
3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[<80685ef4>] (fsg_main_thread) from [<8014bb1c>] (kthread+0x148/0x150)
[<8014bb1c>] (kthread) from [<801010e8>] (ret_from_fork+0x14/0x2c)
Exception stack(0x86623fb0 to 0x86623ff8)
3fa0:                                     00000000 00000000 00000000 00000000
3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
3fe0: 00000000 00000000 00000000 00000000 00000013 00000000
Code: e5974084 e3e03000 e59020cc e3a05000 (e5c43050)  
---[ end trace 28e3678b23d9a982 ]---

- initramfs execute linuxrc script which starts seats in the endless loop waiting for UTP device

Run /linuxrc as init process
uuc 0.6 [built Feb 27 2023 05:09:57]
UTP: Waiting for /dev/utp to appear

 

Does anyone have an experience in the flashing process for SOLO CPU enough to figure out what is wrong?   Maybe someone has kernel-DTB-initramfs based on 4.19.35 kernel suitable for  SOLO CPU?

I appreciate any help on this.

 

0 Kudos
Reply
1 Reply

1,030 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
How you are flashing the image. We will recommend you use the UUU tool with the latest version.
Kindly share the whole log file with us for further debugging of the issue.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply