iMX6 solo HDMI max length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 solo HDMI max length

852 Views
aabhishekoct18
Contributor III

What should be the max  length of HDMI trace if we are ensuring that trace lengths are  matching within spec.

Labels (1)
0 Kudos
Reply
3 Replies

773 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Abhishek Singh,

The HDMI standard specification does not define a maximum trace length, it just defines impedance, so it can be relatively long unlike DDR for example when it’s much more constrained.


I hope this helps!
Regards,

0 Kudos
Reply

773 Views
aabhishekoct18
Contributor III

Thanks for feedback .

Currently my trace length is  326 mil. If this  much length is okay. What preacution / care  i should  take for routing these  traces.

0 Kudos
Reply

773 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Abhishek Singh,

From what I understand that trace length should nor cause problems provided that the impedance is correct. I would also check the HDMI standard for more guidance and as with any trace it’s important to make sure that the EMI is controlled by having a ground signal parallel to the signal trace.

I hope this helps!

Regards,

0 Kudos
Reply