iMX6 eMMC device timeout on first CMD8 (SEND_EXT_CSD)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 eMMC device timeout on first CMD8 (SEND_EXT_CSD)

10,763件の閲覧回数
colinwernham
Contributor II

The eMMC device on my board (using imx6 SOM) fails the CMD8 stage of the JEDEC protocol (JESD84-B451).

It successfully goes through the protocol up-to that point, which uses the CMD line to send CMDx and receive RESPs, but when attempting to get the extended CSD, it times-out, ie nothing received on the DAT0 line.

The device is in the correct TRANS state (set by the preceding CMD7), and after the timeout and error recovery the device state is still in the TRANS state.

The board has an SDCARD on SDIO2 and eMMC (Micron MTFC4GACAANA-4M) on SDIO3

The /drivers/mmc/mmc.c and fsl_esdhc.c debug trace is below, along with the board emmc initialisation.

Any help solving this would be appreciated!

Colin Wernham

---------------------------------------------------------------------------------------------------

U-Boot > mmc dev 1

~~~ mmc_start_init:1274

~~~ mmc_start_init:1278

~~~ mmc_set_clock:789 clock=400000 (f_min=400000,f_max=52000000)

~~~ mmc_start_init:1280 err=0

~~~ mmc_start_init:1284 err=0

~~~ mmc_set_clock:789 clock=400000 (f_min=400000,f_max=52000000)

CMD_SEND:0

                ARG                      0x00000000

                RETURNED                         0 ok

                MMC_RSP_NONE

CMD_SEND:8

                ARG                      0x000001AA

~~~ esdhc_send_cmd:361 IRQSTAT_CTOE irqstat=0x00010000

                RETURNED                         -19 !ERROR!

                MMC_RSP_R1,5,6,7         0x00000003

CMD_SEND:55

                ARG                      0x00000000

~~~ esdhc_send_cmd:361 IRQSTAT_CTOE irqstat=0x00010000

                RETURNED                         -19 !ERROR!

                MMC_RSP_R1,5,6,7         0x00000003

CMD_SEND:0

                ARG                      0x00000000

                RETURNED                         0 ok

                MMC_RSP_NONE

CMD_SEND:1

                ARG                      0x00000000

                RETURNED                         0 ok

                MMC_RSP_R3,4             0x00FF8080

CMD_SEND:1

                ARG                      0x40300000

                RETURNED                         0 ok

                MMC_RSP_R3,4             0x00FF8080

CMD_SEND:1

                ARG                      0x40300000

                RETURNED                         0 ok

                MMC_RSP_R3,4             0xC0FF8080

CMD_SEND:2

                ARG                      0x00000000

                RETURNED                         0 ok

                MMC_RSP_R2               0xFE014E50

                                         0x31585858

                                         0x581229F3

                                         0x9DE4C100

                                        DUMPING DATA

                                        000 - FE 01 4E 50

                                        004 - 31 58 58 58

                                        008 - 58 12 29 F3

                                        012 - 9D E4 C1 00

CMD_SEND:3

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R1,5,6,7         0x00000500

CMD_SEND:9

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R2               0xD04F0132

                                         0x0F5913FF

                                         0xFFFFFFE7

                                         0x8A400000

                                        DUMPING DATA

                                        000 - D0 4F 01 32

                                        004 - 0F 59 13 FF

                                        008 - FF FF FF E7

                                        012 - 8A 40 00 00

CMD_SEND:13

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R1,5,6,7         0x00000700

CURR STATE:3  [STANDBY]

~~~ mmc_startup:899 err=0 mmc->version=66560

~~~ mmc_set_clock:789 clock=20000000 (f_min=400000,f_max=52000000)

~~~ mmc_startup:942 clock=20000000

~~~ mmc_startup:943 tran_speed=25000000

~~~ mmc_startup:944 freq=1000000

~~~ mmc_startup:945 mult=25

~~~ mmc_startup:946 MMC_MAX_BLOCK_LEN=512

~~~ mmc_startup:947 read_bl_len=512

~~~ mmc_startup:948 write_bl_len=512

~~~ mmc_startup:949 high_capacity=1

~~~ mmc_startup:950 csize=1

~~~ mmc_startup:951 cmult=1

~~~ mmc_startup:952 capacity_user=512

CMD_SEND:7

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R1,5,6,7         0x00000700

CMD_SEND:13

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R1,5,6,7         0x00000900

CURR STATE:4   [TRANS]

CMD_SEND:8     [<<----CMD8 FAILS]

                ARG                      0x00000000

~~~ esdhc_send_cmd:413 IRQSTAT_DTOE irqstat=0x00100001

                RETURNED                         -19 !ERROR!

                MMC_RSP_R1,5,6,7         0x00000900

CMD_SEND:13

                ARG                      0x00010000

                RETURNED                         0 ok

                MMC_RSP_R1,5,6,7         0x00000900

CURR STATE:4  [TRANS]

mmc1 is current device

U-Boot >

---------------------------------------------------------------------------------------------------

In the board file:

#define USDHC_PAD_CTRL (PAD_CTL_PUS_47K_UP |        \

    PAD_CTL_SPEED_LOW | PAD_CTL_DSE_80ohm |         \

    PAD_CTL_SRE_FAST  | PAD_CTL_HYS)

:

:

  MX6QDL_SET_PAD(PAD_SD3_CLK__USDHC3_CLK   , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_CMD__USDHC3_CMD   , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT0__USDHC3_DAT0 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT1__USDHC3_DAT1 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT2__USDHC3_DAT2 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT3__USDHC3_DAT3 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT4__USDHC3_DAT4 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT5__USDHC3_DAT5 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT6__USDHC3_DAT6 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_DAT7__USDHC3_DAT7 , MUX_PAD_CTRL(USDHC_PAD_CTRL));

  MX6QDL_SET_PAD(PAD_SD3_RST__USDHC3_RST   , MUX_PAD_CTRL(USDHC_PAD_CTRL));

/*        MX6QDL_SET_PAD(PAD_GPIO_18__USDHC3_VSELECT, MUX_PAD_CTRL(USDHC_PAD_CTRL));*/

  usdhc3_cfg.max_bus_width = 8;

  usdhc3_cfg.sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);

  fsl_esdhc_initialize(bis, &usdhc3_cfg);

---------------------------------------------------------------------------------------------------

タグ(2)
4 返答(返信)

8,066件の閲覧回数
clementmartin
Contributor II

I got the same trouble with u-boot 2017, but with the same board, the same iomux and the same board files, u-boot 2015 is working... May I miss an CONFIG_XXX option somewhere but I can't found it. It's seems that /drivers/mmc.c as changed a little with frequency, but I don't find something which could be responsible of this

0 件の賞賛
返信

8,066件の閲覧回数
simonecumar
Contributor II

Is there a resolution of this issue?

0 件の賞賛
返信

8,066件の閲覧回数
greghuber
Contributor II

Was there any resolution to this issue? I am having a similar problem with a similar Micron eMMC part on the LS1021A eSDHCI bus. In my case, U-Boot can read the part and load the kernel into memory. The kernel starts booting but I get the same CMD8 failure when the kernel first attempts to access the root file system on the eMMC chip. More details can be provided if necessary.

Thank You.

Greg

8,064件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Colin

it looks like hardware issue, one can check emmc voltages signals

by oscilloscope, as seems it does not output any data.

Also one can try baremetal test (attached part of i.MX6 SDK).

Where is the iMX6 Platform SDK maintained?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信