iMX6 WebGL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 WebGL?

2,675 Views
woutervh
Contributor IV

I have a custom board, with a morty based yocto image.
I want to test the WebGL capabilities. Somebody knows what the prerequisities are?
If possible, I'm using a qtwebkit browser, running without x (eglfs platform)

0 Kudos
Reply
3 Replies

2,283 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Wouter,

WebGL is supported for a long time in our Yocto and Android releases; it is built into our yocto/android BSP releases.

You can use it directly.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,283 Views
woutervh
Contributor IV

Also in the community-based yocto?
What browser do you need for webgl to work?

0 Kudos
Reply

2,283 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Wouter,

All the information regarding Community BSP should be checked on the release notes documentation or mailing list; you could take a look at the following links:

https://community.nxp.com/docs/DOC-99985

http://freescale.github.io/

Regarding supported browsers on official BSP, we tested for Chrome and QT WebEngine; for other browsers, it should work from theory, but we didn't test it.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply