iMX6 UL Suspend Mode Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 UL Suspend Mode Question

3,265 Views
davidweidman
Contributor I

In SUSPEND mode shown in attachment, are these measurements with the IO banks turned on or off?

According to the data sheet the max current for the IO banks is: Imax = N x C x V x (0.5 x F). When we enter SUSPEND mode none of our IO should be toggling so this current goes to zero, however there has to be some quiescent current for each IO bank. Do you have that number or is that included in the total 0.56mW for SUSPEND mode?

Labels (2)
0 Kudos
Reply
3 Replies

3,078 Views
Yuri
NXP Employee
NXP Employee

Hello,

Only I/O leakage may take place in Suspend DSM mode, which is negligible

and not specified.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,078 Views
davidweidman
Contributor I

Just to verify, keeping the IO voltages on in Suspend DSM mode, should have a negligible impact on the 0.58W number?

0 Kudos
Reply

3,078 Views
Yuri
NXP Employee
NXP Employee

Hi,

  Yes, but SUSPEND (DSM) mode means also "High-speed peripheral are powered off".

Regards,

Yuri.

0 Kudos
Reply