iMX6 Solox UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 Solox UART

1,868 次查看
vinythambi
Contributor I

In iMX6 SoloX development board design(SPF-27962), UART1 and UART2 are dedicated for A9 and M4 respectively. Does these pins have to be maintained for custom boards design or debug UART can be changed to any of the other UARTs available?

标签 (1)
0 项奖励
回复
1 回复

1,795 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,
Debug UARTs could be changed, but it is required to consider all the proper settings. Please refer to the following Community threads for details:
imx6 debug uart change 
Change debug UART 
imx6q change uboot debug uart 1 to uart 2 

The main issue of not having externally available the UART1 could be in case of requiring the Serial Downloader Mode by UART instead of by USB, because the serial downloader UART cannot be changed on the ROM code.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复