iMX6 Solo/DualLite processor schematic/PCB symbol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Solo/DualLite processor schematic/PCB symbol

ソリューションへジャンプ
36,224件の閲覧回数
cliverolston
Contributor III

Does anyone know where I can get a schematic/PCB symbol for the iMX6 Solo/DualLite processor?

1 解決策
24,687件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Clive,

I can't find how to save the library as *.llb, but I managed to save it in 16.2 format. I'm also attaching sch-27516 in 16.2 in case you want to extract something from there. About the pcb symbol, allegro doesn't seem to have the option to save it as an old version, but I saved it as *.brd instead of *.dra. If this doesn't work for you I'll try to find an alternative.

Best regards.

Jorge.

元の投稿で解決策を見る

46 返答(返信)
12,251件の閲覧回数
borissnajder
Contributor I

I'm working on a new design with iMX6, and we are targeting to use iMX6 Dual POP package. Is there schematic symbol and/or footprint available for this device (MCIMX6D5EZK08AD).

Regards,

Boris Snajder

0 件の賞賛
返信
12,251件の閲覧回数
EricsEah
Contributor I

Can you help to convert the schematic from orcad 16 version to orcad ver10?

I have an older version and cannot open the new version

0 件の賞賛
返信
12,251件の閲覧回数
peterhygren
Contributor II

Here's the layout in Altium format for the SABRE Board for Smart Devices Based on the i.MX 6 Series Product Summary Page revision C3.

https://dl.dropboxusercontent.com/u/109867706/EVALBOARD_20130430.zip

If you want the footprints: Tools => Make integrated library.

0 件の賞賛
返信
12,251件の閲覧回数
alexandereshuis
Contributor I

Dear Peter,

could u please send the Altium format for the SABRE Board for Smart Devices Based on the i.MX 6 Series Product Summary Page revision C3.

it nowadays gives a 404

thanks in advance

0 件の賞賛
返信
12,251件の閲覧回数
peterhygren
Contributor II

Hi Alexander,

I've uploaded the file to this site, but it has to be approved by a moderator before it's visible. I'll check in later to see if it's been approved. I think you should be able to find it as well as posted by me as soon as it's approved.

Regards,

Peter

0 件の賞賛
返信
12,251件の閲覧回数
alexandereshuis
Contributor I

Dear Peter,


Thanks for  the PCB however, Tools => Make integrated library. does not work (most likely because no schematic ) 


Do you by any chance have the altium schematic as well??

So l can fetch the actual fetch the integrated library from the board?


0 件の賞賛
返信
12,251件の閲覧回数
peterhygren
Contributor II

Which symbol is it that you require?

I'm sorry but I don't have the schematic part saved, but I did convert a number of the parts on the board.

0 件の賞賛
返信
12,251件の閲覧回数
alexandereshuis
Contributor I

The quad imx6

Would be most helpfull

Verstuurd vanaf mijn iPhone

Op 10 sep. 2013 om 16:33 heeft "Peter Hygren" <[email protected]> het volgende geschreven:

iMX6 Solo/DualLite processor schematic/PCB symbol

reply from Peter Hygren in i.MX Community - View the full discussion

Which symbol is it that you require?

I'm sorry but I don't have the schematic part saved, but I did convert a number of the parts on the board.

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

Following iMX6 Solo/DualLite processor schematic/PCB symbol in these streams: Inbox

0 件の賞賛
返信
12,249件の閲覧回数
peterhygren
Contributor II

Attaching footprint and symbol library for IMX6Q and IMX6D (they share symbol and footprint).

In the PCB library I've added 2 footprints for the processor, one extracted from the SABRE Smart Devices board, and one I created myself. The symbol is linked to the footprint I created, and it's been verified to work on a number of boards now with no complaints from assembly line.

Regards,

Peter Hygren

0 件の賞賛
返信
12,249件の閲覧回数
_carlos
Contributor I

Hi,

does anybody have a symbol/footprint for the iMX6 Quad version?

cheers Karl

0 件の賞賛
返信
12,250件の閲覧回数
peterhygren
Contributor II

What's with all the missing pads?bga.png

0 件の賞賛
返信
12,249件の閲覧回数
cliverolston
Contributor III

Hi Peter,

This footprint is for the i.MX6 SoloLite. I've asked Yuri for the Solo/DualLite footprint - see my previous post.

Cheers,

Clive

0 件の賞賛
返信
12,249件の閲覧回数
Yuri
NXP Employee
NXP Employee

The attached relates to MX6 with part number PCIMX6U8DVM10AA,

package MAPBGA 21x21 0.8mm.

12,249件の閲覧回数
cliverolston
Contributor III

Yuri, works a treat. Thanks, Clive

0 件の賞賛
返信
12,249件の閲覧回数
Rob_iMX6
Contributor II

Hi Clive

How did you manage to get the symbol into Altium Designer? The importer simply say "not recognized"...

Could you please upload you AD version? Thanks a lot!

Best regards,

-Rob

0 件の賞賛
返信
12,249件の閲覧回数
cliverolston
Contributor III

Hi Rob,

Here's the Altium symbol and the footprint. The footprint's missing the dimensions at present.

Cheers,

Clive

12,249件の閲覧回数
daviduhen
Contributor I

Clive and Rob,

I am traveling the same path you did with Yuri's files.  Any chance you can post the complete Altium Project of the imported Ref Design?

Regards,

DAU

0 件の賞賛
返信
12,248件の閲覧回数
cliverolston
Contributor III

Hi David,

Here's the Altium project zip file. Is this what you wanted?

Cheers,

Clive

0 件の賞賛
返信
12,248件の閲覧回数
daviduhen
Contributor I

Thanks for the file Clive.  I am trying to put together a complete Altium project - schematics plus pcb with cross probing nets.  I have started with SCH-27516_16_2 but I'm not sure which PCB matches.  Can you explain the numbering?  I have documents with the following numbers 27516, 27392, 27417, 27452.  Are there descriptions of each of these somewhere?

Regards,

DAU

0 件の賞賛
返信
12,248件の閲覧回数
Rob_iMX6
Contributor II

Hi Clive

Thank you very much! I owe you a beer or two!

Kind regards,

-Rob

0 件の賞賛
返信