iMX6 Solo/DualLite processor schematic/PCB symbol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Solo/DualLite processor schematic/PCB symbol

ソリューションへジャンプ
35,803件の閲覧回数
cliverolston
Contributor III

Does anyone know where I can get a schematic/PCB symbol for the iMX6 Solo/DualLite processor?

1 解決策
24,266件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Clive,

I can't find how to save the library as *.llb, but I managed to save it in 16.2 format. I'm also attaching sch-27516 in 16.2 in case you want to extract something from there. About the pcb symbol, allegro doesn't seem to have the option to save it as an old version, but I saved it as *.brd instead of *.dra. If this doesn't work for you I'll try to find an alternative.

Best regards.

Jorge.

元の投稿で解決策を見る

46 返答(返信)
1,852件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the enclosed.

1,851件の閲覧回数
cliverolston
Contributor III

Hi Yuri,

This layout appears to be using the iMX6 Solo Lite 24 x 24 ball package. I was looking for the Solo/DualLite 25 x 25 ball package.

Cheers,

Clive

0 件の賞賛
返信
1,852件の閲覧回数
cliverolston
Contributor III

Thanks very much Jorge. The import in 16.2 format to Altium worked a treat.

Cheers,

Clive

0 件の賞賛
返信
1,852件の閲覧回数
admin
Specialist II

Clive, try checking on this page and let me know if you don't find what you are looking for for the Solo/DualLite.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&nodeId=018rH3ZrDRB24A&fpsp=1&...

Regards,

Grant

0 件の賞賛
返信
1,852件の閲覧回数
PradapRaj
Contributor III

Hi Clive Rolston,

Now i.MX6 documentation and design files are avilable to public. You can access all the files from the below Freescale webpage link. Duallite design files are available under i.MX6_SABRE_SDP_DESIGNFILES.

i.MX6Q Product Summary Page

Regards,

Pradap

0 件の賞賛
返信