iMX6 SRTC Mode GPIO State

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 SRTC Mode GPIO State

1,637 Views
johnson_dana
Contributor II

When we put the iMX6 in SRTC mode (deepest of all the sleep modes), we see current leakage paths through the iMX6. For instance we have an open drain inverter with a pullup(10k to 3.3V) on inverter output. That output goes to an iMX6 GPIO and the sleep current while in SRTC mode exceeds 40 mA, so many circuits within the iMX6 are being powered. We noticed that on VDD_3V after the PMIC was powered down, VDD_3V still had about 1.79V. Disconnecting the signal with the 10k pullup from the iMX6 entirely, results in sub 1 mA sleep currents.

Is there a way to set the GPIO to high impedance while in SRTC? I don’t think it’s possible but need to ask the question. Our backup solution is to add a buffer between the pullup and iMX6 GPIO. That buffer would be turned off completely when we enter SRTC mode.

Labels (3)
0 Kudos
Reply
1 Reply

1,590 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dana

you are right: there is no way to set the GPIO to high impedance while in SRTC.

It is not allowed to connect powered external devices to unpowered processor, also

it violates power-up sequence described in sect.4.2.1 Power-Up Sequence datasheet

i.MX 6Solo/6DualLite Applications Processors for Consumer Products

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply