iMX6 RGMII TskewT impact on Receive side

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 RGMII TskewT impact on Receive side

1,327件の閲覧回数
xdumoulin
Contributor III

Hi,

Between the iMX6 Dual Lite and iMX6 Quad datasheet, in the RGMII Signal Switching Specifications, the TskewT parameter change from -500ps / +500ps (Dual Lite) to -100ps / +900ps (Quad).

This change will obviously have an impact on the RGMII Transmit side. But will it have an impact as well on the Receive side ? Figure 48 from Quad Datasheet (or Figure 53 from Dual Lite Datasheet) seems to show an impact on the receive side.

Thanks,

Xavier

ラベル(2)
0 件の賞賛
返信
1 返信

1,260件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

TskewR is the same for both i.MX6Q and DualLite according to

Table  RGMII Signal Switching Specifications

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf 

Difference in TskewTmay be explained by different transmit path as silicon

die is different for both chips. Receiver just latches data in buffer and there is no difference.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信