iMX6 RGMII TskewT impact on Receive side

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 RGMII TskewT impact on Receive side

1,305 Views
xdumoulin
Contributor III

Hi,

Between the iMX6 Dual Lite and iMX6 Quad datasheet, in the RGMII Signal Switching Specifications, the TskewT parameter change from -500ps / +500ps (Dual Lite) to -100ps / +900ps (Quad).

This change will obviously have an impact on the RGMII Transmit side. But will it have an impact as well on the Receive side ? Figure 48 from Quad Datasheet (or Figure 53 from Dual Lite Datasheet) seems to show an impact on the receive side.

Thanks,

Xavier

Labels (2)
0 Kudos
Reply
1 Reply

1,238 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

TskewR is the same for both i.MX6Q and DualLite according to

Table  RGMII Signal Switching Specifications

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf 

Difference in TskewTmay be explained by different transmit path as silicon

die is different for both chips. Receiver just latches data in buffer and there is no difference.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply