iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

34,433 Views
tarterkit_ru
Contributor III

As see on shematic few iMX6 boards, RGMII PHY put to MAC 125MHz to ENET_REF_CLK/ENET_TX_CLKENET_TX_CLK pin.

What it for?

I can't see any describe of this in manuals and RGMII not require this signal.

Labels (3)
21 Replies

19,987 Views
fei_liu
NXP Employee
NXP Employee

In RGMII Mode, only the pin "ENET_REF_CLK" could used as 125M reference clock input.

The 125M reference clock could be from PHY chip, or external oscillator, and could also be routed from GPIO_16(need software configuration).

In RMII Mode, only two pins "GPIO_16" and "RGMII_TX_CTL" could be used as the 50M reference clock. The clock source could be from external oscillator or internal PLL, need software configuration. Please refer the document "I.MX6 Hardware Development Guide", Chapter 11.

0 Kudos
Reply

19,987 Views
yinchunhui
Contributor II

hello Fei Liu

You said "The 125M reference clock could be from PHY chip, or external oscillator, and could also be routed from GPIO_16(need software configuration)."

I want to ask how to routed from GPIO_16?What is the detail configuration?

Now I can generate the 125M clock at the GPIO_16.

Thank you very much

0 Kudos
Reply

19,987 Views
fei_liu
NXP Employee
NXP Employee

ENET_REF_CLK is the input pin for RGMII reference clock, so if you want to use GPIO_16 to provide the 125M clock, you should connect GPIO_16 to ENENT_REF_CLK, and be careful, the voltage level might be different, you might need an level shift.

0 Kudos
Reply

19,987 Views
yinchunhui
Contributor II

thank you very much!

But I see you say"need software configuration",is there any method though software?

0 Kudos
Reply

19,976 Views
fei_liu
NXP Employee
NXP Employee

The software configuration is just for outputting 125M on GPIO_16, since you have already done, no additional operations or configurations are needed.

Best regards,

Frank Liu

0 Kudos
Reply

19,944 Views
yinchunhui
Contributor II

ok,I know,thank you very much!

19,987 Views
MaxChou
Contributor III

Hi Fei Liu

We follow "I.MX6 Hardware Development Guide", Chapter 11,

and modify below pin for RMII interface

////////////////

MX6Q_PAD_ENET_CRS_DV__ENET_RX_EN,

MX6Q_PAD_ENET_MDIO__ENET_MDIO,

MX6Q_PAD_ENET_MDC__ENET_MDC,

MX6Q_PAD_ENET_TX_EN__ENET_TX_EN,

MX6Q_PAD_ENET_TXD0__ENET_TDATA_0,

MX6Q_PAD_ENET_TXD1__ENET_TDATA_1,

MX6Q_PAD_ENET_RXD0__ENET_RDATA_0,

MX6Q_PAD_ENET_RXD1__ENET_RDATA_1,

MX6Q_PAD_ENET_RX_ER__ENET_RX_ER,

MX6Q_PAD_RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT,

//////////////////

but we still have problem on RMII,

is anything else I should check in the kernel driver ??

How to config below pins ? Should I modify it to other function ??

/////////////////////////////////////////////////// 
MX6Q_PAD_RGMII_TXC__ENET_RGMII_TXC,
MX6Q_PAD_RGMII_TD0__ENET_RGMII_TD0,
MX6Q_PAD_RGMII_TD1__ENET_RGMII_TD1,
MX6Q_PAD_RGMII_TD2__ENET_RGMII_TD2,
MX6Q_PAD_RGMII_TD3__ENET_RGMII_TD3,
MX6Q_PAD_RGMII_RXC__ENET_RGMII_RXC,
MX6Q_PAD_RGMII_RD0__ENET_RGMII_RD0,
MX6Q_PAD_RGMII_RD1__ENET_RGMII_RD1,
MX6Q_PAD_RGMII_RD2__ENET_RGMII_RD2,
MX6Q_PAD_RGMII_RD3__ENET_RGMII_RD3,
MX6Q_PAD_RGMII_RX_CTL__ENET_RGMII_RX_CTL,

/////////////////////////////////////////////////////

Sincerely,Max

0 Kudos
Reply

19,987 Views
DuanFugang
NXP Employee
NXP Employee

Kernel driver don’t support RMII, but we have patch for this. (You can email to me to get it: [email protected])

Don’t care about RGMII pad control.



0 Kudos
Reply

19,986 Views
DuanFugang
NXP Employee
NXP Employee

Attached the patch for RMII base on kernel 3.0.35.

19,986 Views
liguoqing
Contributor I

Hi Duan

How can i use RMII on imx6D on kernel 4.1.15?

0 Kudos
Reply

19,986 Views
marcocavallini
Contributor V

For RMII you need to set 50Mhz clock for enet, the best option would be to set it in u-boot using the following call and have the clock already set in the kernel

enable_fec_anatop_clock(ENET_50MHZ);‍‍
0 Kudos
Reply

19,986 Views
mchaplet
Contributor II

Thanks for this patch !

I also use LAN8720 and RMII connection to it from a IMX6S and it works well in U-Boot but last kernel 3.10.17 from imx git seems to disable 50MHz PLL.

How to force it in DTS ?

I've yet tried to replace clks190 - "ptp" by "enet_ref" in fec controller description (imx6qdl.dtsi) without success.

Thanks,

Martin

0 Kudos
Reply

19,986 Views
marcocavallini
Contributor V

Hi,

is it working your i.MX6S kernel 3.10.17 with LAN8720 and RMII connection?

0 Kudos
Reply

19,986 Views
shabeerbadarudh
Contributor IV

sorry for the late reply.

Yes, it was worked in our platform. (i.MX6S kernel 3.10.17 with LAN8720 and RMII)

0 Kudos
Reply

19,986 Views
marcocavallini
Contributor V

Here it is at last ;-)

Cordiali Saluti / Kindest Regards / Mit freundlichen Grüßen

--

Marco Cavallini | KOAN sas | Bergamo - Italia

embedded and real-time software engineering

Phone:+39-035-255.235 - Fax:+39-178-22.39.748

0 Kudos
Reply

19,986 Views
shabeerbadarudh
Contributor IV

Hi Martin,

We are also facing the same issue. Did you have any luck in 3.10.17?

0 Kudos
Reply

19,986 Views
lukascaha
Contributor I

hello,

we have similar problem with custom board with MX6S/DL. PHY is LAN8720 and i u-boot works ok.

In kernel, iomux and clock generated by gpio_16 is ok.

I don't understand - kernel driver don't support RMII, but on MX6SL dev board (and processor) is only RMII.

I know this is allmost another processor, but changes in u-boot are inpired by mx6slevk.c

Ist about RMII support for MX6S/DL/Q ?

For what kernel branch is patch applicable - is RMII support better in some branches - I use imx_3.0.35_1.1.0

thank

Lukas

0 Kudos
Reply

19,986 Views
MaxChou
Contributor III

Hi Fugang Duan

it is sloved, thanks!!

0 Kudos
Reply

19,971 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Pavel,

There are 3 ways to supply the ENET clock. Please see chapter 11 of the attached, I think it will clarify.

Best regards.

Jorge.

19,971 Views
tarterkit_ru
Contributor III

Thanks, this document told about GPIO_16 refclock connections, but sabresd, sabresdlite boards use ENET_REF_CLK pin for reference clock and this document don't have any for it ...

0 Kudos
Reply