iMX6 - ESAI and SSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 - ESAI and SSI

1,760 Views
markusmayer
Contributor I

Hallo all!

I'm currently working on block diagram and I have to connect the audio interfaces to the external

peripherals.

Where can I find the mapping of the ESAI/SSI to the pins of the iMX6? In the datasheet I haven't

found these information ....

best regards

Labels (1)
0 Kudos
Reply
1 Reply

1,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi Markus

for mapping details one can look at documentation for each

processor, for example for i.MX6Q:

Chapter 4 External Signals and Pin Multiplexing, Table 25-1. ESAI External Signals

Chapter 16 Digital Audio Multiplexer (AUDMUX) i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

SSI has not external signals it is routed through AUDMUX, use Table 85. AUDMUX Port Allocation

i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply