iMX6 Dual PCIe Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Dual PCIe Question

1,273件の閲覧回数
davidboudreau
Contributor I

I am going to use the PCIe function on the iMX6 Dual Processor. I plan on using the iMX6 signal CLK1_N (ball C7) for the PCIe signal REFCLK- and the iMX6 signal CLK1_P (ball D7) for the PCIe signal REFCLK+. Does this differential clock signal have to be AC coupled? They are AC coupled on the Sabre PCBA but i"m not sure if that is correct.

0 件の賞賛
返信
1 返信

1,114件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi David

it may be coupled directly provided that datasheet

LVDS I/O DC Parameters will be satisfied.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信