iMX6 CTS test fail: testChangeSubtitleTrack/testDeselectTrack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 CTS test fail: testChangeSubtitleTrack/testDeselectTrack

2,475 Views
rockleeuic
Contributor I

Hi, FSL,

   When test CTS 4.4.r4 in iMX6 (KK4.4.2), we got failed in the two items:  testChangeSubtitleTrack, testDeselectTrack in android.media.cts.MediaPlayerTest.  Is there any wrong in our settings ?

====================================

E/BufferQueue( 2067): [com.android.cts.media/android.media.cts.MediaStubActivity] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

D/OpenGLRenderer( 3221): Enabling debug mode 0

I/ActivityManager( 2451): Displayed com.android.cts.media/android.media.cts.MediaStubActivity: +523ms

I/OMXCodec( 2070): [OMX.Freescale.std.video_decoder.h263.hw-based] video dimensions are 352 x 288

E/MediaPlayer( 3221): Should have subtitle controller already set

I/vpu-lib ( 2070): Product Info: i.MX6Q/D/S

I/vpu-lib ( 2070): <gpu> alloc handle: 0x41aaeb28, paddr: 0x160fe000, vaddr: 0x4555c000

I/vpu-lib ( 2070): <gpu> alloc handle: 0x41aaeb50, paddr: 0x135d4000, vaddr: 0x42a32000

I/vpu-lib ( 2070): bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0

W/vpu-lib ( 2070): VPU iram is less than needed, some parts don't use iram

I/OMXCodec( 2070): [OMX.Freescale.std.video_decoder.h263.hw-based] video dimensions are 352 x 288

I/OMXCodec( 2070): [OMX.Freescale.std.video_decoder.h263.hw-based] Crop rect is 352 x 288 @ (0, 0)

I/vpu-lib ( 2070): <gpu> alloc handle: 0x41aaed78, paddr: 0x13980000, vaddr: 0x42dde000

D/MediaPlayerTest( 3221): text: 0:0000, trackId: 0, posMs: 0

I/AudioMixer( 2070): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

W/audio_hw_primary( 2070): card 0, port 0 device 0x2

W/audio_hw_primary( 2070): rate 48000, channel 2 period_size 0xc0

W/MediaPlayer( 3221): info/warning (3, 0)

E/OMXCodec( 2070): [OMX.Freescale.std.video_decoder.h263.hw-based] dequeueBuffer failed w/ error 0xfffffff0

D/MediaPlayerTest( 3221): text: 0:1000, trackId: 0, posMs: 986

D/MediaPlayerTest( 3221): text: 1:500, trackId: 1, posMs: 986

D/MediaPlayerTest( 3221): text: 1:1500, trackId: 1, posMs: 1421

F/        ( 2070): frameworks/av/media/libstagefright/foundation/AString.cpp:128 CHECK(mSize > 0) failed.

F/libc    ( 2070): Fatal signal 6 (SIGABRT) at 0x00000816 (code=-6), thread 3235 (TimedTextDriver)

I/DEBUG   ( 2066): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

I/DEBUG   ( 2066): AM write failure (32 / Broken pipe)

I/DEBUG   ( 2066): Build fingerprint: 'UIC/nPOS15/nPOS15:4.4.2/101.06/20151216:user/dev-keys'

I/DEBUG   ( 2066): Revision: '397330'

I/DEBUG   ( 2066): pid: 2070, tid: 3235, name: TimedTextDriver  >>> /system/bin/mediaserver <<<

I/DEBUG   ( 2066): signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------

W/NativeCrashListener( 2451): Couldn't find ProcessRecord for pid 2070

I/DEBUG   ( 2066):     r0 00000000  r1 00000ca3  r2 00000006  r3 00000000

I/DEBUG   ( 2066):     r4 00000006  r5 00000000  r6 00000ca3  r7 0000010c

I/DEBUG   ( 2066):     r8 41cadc58  r9 419ea8a8  sl 41cadc50  fp 4020f2ec

I/DEBUG   ( 2066):     ip 41cadc1c  sp 41cad750  lr 401d60bd  pc 401e5088  cpsr 000e0010

I/DEBUG   ( 2066):     d0  0000000000000000  d1  0000000000000000

I/DEBUG   ( 2066):     d2  0000000000000000  d3  0000000000000000

I/DEBUG   ( 2066):     d4  3fdbd2e30e84071e  d5  bebbb9c7f5efed7b

I/DEBUG   ( 2066):     d6  3e66376972bea4d0  d7  3ecccccd3ecccccd

I/DEBUG   ( 2066):     d8  0000000000000000  d9  0000000000000000

I/DEBUG   ( 2066):     d10 0000000000000000  d11 0000000000000000

I/DEBUG   ( 2066):     d12 0000000000000000  d13 0000000000000000

I/DEBUG   ( 2066):     d14 0000000000000000  d15 0000000000000000

I/DEBUG   ( 2066):     d16 00000000000010b9  d17 000000000000109e

I/DEBUG   ( 2066):     d18 000000000000001b  d19 bfc1e67084800000

I/DEBUG   ( 2066):     d20 3fc5538dd7e50657  d21 bf66beb60668b211

I/DEBUG   ( 2066):     d22 bfc25135bba773dd  d23 3fe0000000000000

I/DEBUG   ( 2066):     d24 3f831fcbe2734b9e  d25 bf831fcbe901c76b

I/DEBUG   ( 2066):     d26 3f6328e1cb8c85e0  d27 4000000000000000

I/DEBUG   ( 2066):     d28 400125135bba773e  d29 3fc0b473c5efe389

I/DEBUG   ( 2066):     d30 3ff0000000000000  d31 3fdbd2e30e84071e

I/DEBUG   ( 2066):     scr 28000010

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): backtrace:

I/DEBUG   ( 2066):     #00  pc 00022088  /system/lib/libc.so (tgkill+12)

I/DEBUG   ( 2066):     #01  pc 000130b9  /system/lib/libc.so (pthread_kill+48)

I/DEBUG   ( 2066):     #02  pc 000132cd  /system/lib/libc.so (raise+10)

I/DEBUG   ( 2066):     #03  pc 00012003  /system/lib/libc.so

I/DEBUG   ( 2066):     #04  pc 0002193c  /system/lib/libc.so (abort+4)

I/DEBUG   ( 2066):     #05  pc 000014c3  /system/lib/liblog.so (__android_log_assert+86)

I/DEBUG   ( 2066):     #06  pc 0000c76d  /system/lib/libstagefright_foundation.so (android::AString::trim()+96)

I/DEBUG   ( 2066):     #07  pc 0009c4f1  /system/lib/libstagefright.so (android::TimedTextSRTSource::getNextSubtitleInfo(long long*, long long*, android::TimedTextSRTSource::TextInfo*)+240)

I/DEBUG   ( 2066):     #08  pc 0009c535  /system/lib/libstagefright.so (android::TimedTextSRTSource::scanFile()+24)

I/DEBUG   ( 2066):     #09  pc 0009c581  /system/lib/libstagefright.so (android::TimedTextSRTSource::start()+4)

I/DEBUG   ( 2066):     #10  pc 0009d21f  /system/lib/libstagefright.so (android::TimedTextPlayer::onMessageReceived(android::sp<android::AMessage> const&)+822)

I/DEBUG   ( 2066):     #11  pc 00009405  /system/lib/libstagefright_foundation.so (android::ALooperRoster::deliverMessage(android::sp<android::AMessage> const&)+152)

I/DEBUG   ( 2066):     #12  pc 00008edf  /system/lib/libstagefright_foundation.so (android::ALooper::loop()+198)

I/DEBUG   ( 2066):     #13  pc 0000e9ed  /system/lib/libutils.so (android::Thread::_threadLoop(void*)+104)

I/DEBUG   ( 2066):     #14  pc 0000e58f  /system/lib/libutils.so

I/DEBUG   ( 2066):     #15  pc 0000d248  /system/lib/libc.so (__thread_entry+72)

I/DEBUG   ( 2066):     #16  pc 0000d3e0  /system/lib/libc.so (pthread_create+240)

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): stack:

I/DEBUG   ( 2066):          41cad710  00000000 

I/DEBUG   ( 2066):          41cad714  00000000 

I/DEBUG   ( 2066):          41cad718  00000000 

I/DEBUG   ( 2066):          41cad71c  000003ff 

I/DEBUG   ( 2066):          41cad720  00000000 

I/DEBUG   ( 2066):          41cad724  00000000 

I/DEBUG   ( 2066):          41cad728  41cadc1c 

I/DEBUG   ( 2066):          41cad72c  41cadc58 

I/DEBUG   ( 2066):          41cad730  419ea8a8 

I/DEBUG   ( 2066):          41cad734  41cadc50 

I/DEBUG   ( 2066):          41cad738  401440b1  /system/lib/liblog.so

I/DEBUG   ( 2066):          41cad73c  401455f9  /system/lib/liblog.so

I/DEBUG   ( 2066):          41cad740  41cad7b4 

I/DEBUG   ( 2066):          41cad744  00000000 

I/DEBUG   ( 2066):          41cad748  40211384 

I/DEBUG   ( 2066):          41cad74c  401441fd  /system/lib/liblog.so (__android_log_write+212)

I/DEBUG   ( 2066):     #00  41cad750  00000006 

I/DEBUG   ( 2066):          41cad754  00000000 

I/DEBUG   ( 2066):          41cad758  00000ca3 

I/DEBUG   ( 2066):          41cad75c  41cadc1c 

I/DEBUG   ( 2066):          41cad760  41cadc1c 

I/DEBUG   ( 2066):          41cad764  401d60bd  /system/lib/libc.so (pthread_kill+52)

I/DEBUG   ( 2066):     #01  41cad768  00000006 

I/DEBUG   ( 2066):          41cad76c  00000000 

I/DEBUG   ( 2066):          41cad770  00000000 

I/DEBUG   ( 2066):          41cad774  401d62d1  /system/lib/libc.so (raise+14)

I/DEBUG   ( 2066):     #02  41cad778  41cad784 

I/DEBUG   ( 2066):          41cad77c  401d5007  /system/lib/libc.so

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near r8:

I/DEBUG   ( 2066):     41cadc38 41cadccc 41bb0000 41f639d4 4077d539 

I/DEBUG   ( 2066):     41cadc48 00000026 00000000 00000000 00000000 

I/DEBUG   ( 2066):     41cadc58 0007a120 00000000 0000001e 00000000 

I/DEBUG   ( 2066):     41cadc68 41cadccc 401d432f 4020d000 41220fc8 

I/DEBUG   ( 2066):     41cadc78 41220fc8 4074c795 41cadc9c 00000000 

I/DEBUG   ( 2066):     41cadc88 00000000 40732ed3 419ea698 41d29480 

I/DEBUG   ( 2066):     41cadc98 419ea8a8 00000000 405b8020 4077d585 

I/DEBUG   ( 2066):     41cadca8 4077d57d 41d29480 41d29494 4077e221 

I/DEBUG   ( 2066):     41cadcb8 40092a30 412dea08 40269559 401d432f 

I/DEBUG   ( 2066):     41cadcc8 4121f790 419ea8a8 00000018 4121f798 

I/DEBUG   ( 2066):     41cadcd8 00000000 41cadd60 405b801c 41d29100 

I/DEBUG   ( 2066):     41cadce8 405b8020 40269559 41bb0000 41f639d4 

I/DEBUG   ( 2066):     41cadcf8 00000000 405af343 41cadd2c 412067a4 

I/DEBUG   ( 2066):     41cadd08 41cadd60 41d29480 00000000 405b8020 

I/DEBUG   ( 2066):     41cadd18 40269559 405af407 40269559 41d29480 

I/DEBUG   ( 2066):     41cadd28 405b801c 41d29480 41cadd4c 00000001 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near r9:

I/DEBUG   ( 2066):     419ea888 006e0065 0000001b 00000001 00000001 

I/DEBUG   ( 2066):     419ea898 419ea840 00000000 00000067 00000033 

I/DEBUG   ( 2066):     419ea8a8 407ceb40 419ea8d8 419ea840 418bb348 

I/DEBUG   ( 2066):     419ea8b8 00000000 407ceb10 00000000 00000000 

I/DEBUG   ( 2066):     419ea8c8 00000000 00000020 006e0065 0000001b 

I/DEBUG   ( 2066):     419ea8d8 00000004 00000004 419ea8a8 00000000 

I/DEBUG   ( 2066):     419ea8e8 00b30095 0000001b 00000001 00000001 

I/DEBUG   ( 2066):     419ea8f8 418bb348 00000000 009b8090 0000007b 

I/DEBUG   ( 2066):     419ea908 00000001 00000060 00a4009f 809b8097 

I/DEBUG   ( 2066):     419ea918 6c616e67 80a000a2 63737472 00000004 

I/DEBUG   ( 2066):     419ea928 00646e75 00b000a6 00a800a7 809f809e 

I/DEBUG   ( 2066):     419ea938 80a780a3 00ac80a4 00c200ab 80aa80a6 

I/DEBUG   ( 2066):     419ea948 80d000ad 00c900ae 80a900af 00d480a8 

I/DEBUG   ( 2066):     419ea958 00b200b1 80ac80ab 80ae80ad 00bb00b4 

I/DEBUG   ( 2066):     419ea968 00b800b5 00b700b6 80b080af 80b280b1 

I/DEBUG   ( 2066):     419ea978 00ba00b9 0000005b 00000001 00000040 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near sl:

I/DEBUG   ( 2066):     41cadc30 419ea8a8 41cadc48 41cadccc 41bb0000 

I/DEBUG   ( 2066):     41cadc40 41f639d4 4077d539 00000026 00000000 

I/DEBUG   ( 2066):     41cadc50 00000000 00000000 0007a120 00000000 

I/DEBUG   ( 2066):     41cadc60 0000001e 00000000 41cadccc 401d432f 

I/DEBUG   ( 2066):     41cadc70 4020d000 41220fc8 41220fc8 4074c795 

I/DEBUG   ( 2066):     41cadc80 41cadc9c 00000000 00000000 40732ed3 

I/DEBUG   ( 2066):     41cadc90 419ea698 41d29480 419ea8a8 00000000 

I/DEBUG   ( 2066):     41cadca0 405b8020 4077d585 4077d57d 41d29480 

I/DEBUG   ( 2066):     41cadcb0 41d29494 4077e221 40092a30 412dea08 

I/DEBUG   ( 2066):     41cadcc0 40269559 401d432f 4121f790 419ea8a8 

I/DEBUG   ( 2066):     41cadcd0 00000018 4121f798 00000000 41cadd60 

I/DEBUG   ( 2066):     41cadce0 405b801c 41d29100 405b8020 40269559 

I/DEBUG   ( 2066):     41cadcf0 41bb0000 41f639d4 00000000 405af343 

I/DEBUG   ( 2066):     41cadd00 41cadd2c 412067a4 41cadd60 41d29480 

I/DEBUG   ( 2066):     41cadd10 00000000 405b8020 40269559 405af407 

I/DEBUG   ( 2066):     41cadd20 40269559 41d29480 405b801c 41d29480 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near fp:

I/DEBUG   ( 2066):     4020f2cc 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f2dc 00000000 00000000 ffffffff 00000000 

I/DEBUG   ( 2066):     4020f2ec 00000000 00000001 00003fff 00000000 

I/DEBUG   ( 2066):     4020f2fc 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f30c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f31c 00000000 00000000 401d5b25 401d5b21 

I/DEBUG   ( 2066):     4020f32c 401d64d3 401d660d 00000000 4024b3ed 

I/DEBUG   ( 2066):     4020f33c 40c1f931 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f34c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f35c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f36c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f37c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f38c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f39c 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f3ac 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     4020f3bc 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near ip:

I/DEBUG   ( 2066):     41cadbfc 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2066):     41cadc0c 00000000 00000000 00000000 000001f4 

I/DEBUG   ( 2066):     41cadc1c 00000000 00000000 00000000 41d29480 

I/DEBUG   ( 2066):     41cadc2c 419ea8a8 419ea8a8 41cadc48 41cadccc 

I/DEBUG   ( 2066):     41cadc3c 41bb0000 41f639d4 4077d539 00000026 

I/DEBUG   ( 2066):     41cadc4c 00000000 00000000 00000000 0007a120 

I/DEBUG   ( 2066):     41cadc5c 00000000 0000001e 00000000 41cadccc 

I/DEBUG   ( 2066):     41cadc6c 401d432f 4020d000 41220fc8 41220fc8 

I/DEBUG   ( 2066):     41cadc7c 4074c795 41cadc9c 00000000 00000000 

I/DEBUG   ( 2066):     41cadc8c 40732ed3 419ea698 41d29480 419ea8a8 

I/DEBUG   ( 2066):     41cadc9c 00000000 405b8020 4077d585 4077d57d 

I/DEBUG   ( 2066):     41cadcac 41d29480 41d29494 4077e221 40092a30 

I/DEBUG   ( 2066):     41cadcbc 412dea08 40269559 401d432f 4121f790 

I/DEBUG   ( 2066):     41cadccc 419ea8a8 00000018 4121f798 00000000 

I/DEBUG   ( 2066):     41cadcdc 41cadd60 405b801c 41d29100 405b8020 

I/DEBUG   ( 2066):     41cadcec 40269559 41bb0000 41f639d4 00000000 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): memory near sp:

I/DEBUG   ( 2066):     41cad730 419ea8a8 41cadc50 401440b1 401455f9 

I/DEBUG   ( 2066):     41cad740 41cad7b4 00000000 40211384 401441fd 

I/DEBUG   ( 2066):     41cad750 00000006 00000000 00000ca3 41cadc1c 

I/DEBUG   ( 2066):     41cad760 41cadc1c 401d60bd 00000006 00000000 

I/DEBUG   ( 2066):     41cad770 00000000 401d62d1 41cad784 401d5007 

I/DEBUG   ( 2066):     41cad780 00000000 ffffffdf 00000000 00000000 

I/DEBUG   ( 2066):     41cad790 00000000 7d27823d 00000000 00000000 

I/DEBUG   ( 2066):     41cad7a0 00000000 401e4940 401440b1 401444c7 

I/DEBUG   ( 2066):     41cad7b0 41cadbc4 6d617266 726f7765 612f736b 

I/DEBUG   ( 2066):     41cad7c0 656d2f76 2f616964 7362696c 65676174 

I/DEBUG   ( 2066):     41cad7d0 67697266 662f7468 646e756f 6f697461 

I/DEBUG   ( 2066):     41cad7e0 53412f6e 6e697274 70632e67 32313a70 

I/DEBUG   ( 2066):     41cad7f0 48432038 284b4345 7a69536d 203e2065 

I/DEBUG   ( 2066):     41cad800 66202930 656c6961 41002e64 00000000 

I/DEBUG   ( 2066):     41cad810 4020cfd8 00000001 4021b324 40211384 

I/DEBUG   ( 2066):     41cad820 40207446 40207446 00000000 00000000 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): code around pc:

I/DEBUG   ( 2066):     401e5068 e8bd00f0 e3700a01 912fff1e e2600000 

I/DEBUG   ( 2066):     401e5078 ea006f0a e92d50f0 e3a07f43 ef000000 

I/DEBUG   ( 2066):     401e5088 e8bd50f0 e3700a01 912fff1e e2600000 

I/DEBUG   ( 2066):     401e5098 ea006f02 e92d50f0 e3a070ee ef000000 

I/DEBUG   ( 2066):     401e50a8 e8bd50f0 e3700a01 912fff1e e2600000 

I/DEBUG   ( 2066):     401e50b8 ea006efa e1520003 8a006f00 e92d4011 

I/DEBUG   ( 2066):     401e50c8 e24dd01c f5d0f000 f5d1f000 f5d1f020 

I/DEBUG   ( 2066):     401e50d8 e3520004 3a0000b7 e2613000 e2133003 

I/DEBUG   ( 2066):     401e50e8 0a000007 e1b0cf83 e0422003 44d13001 

I/DEBUG   ( 2066):     401e50f8 24d14001 24d1c001 44c03001 24c04001 

I/DEBUG   ( 2066):     401e5108 24c0c001 e020c001 e31c0003 1a00002b 

I/DEBUG   ( 2066):     401e5118 e88d0fe0 e2603000 e213301c 0a00000a 

I/DEBUG   ( 2066):     401e5128 e1530002 8202301c e1b0ce03 28b100f0 

I/DEBUG   ( 2066):     401e5138 48b10300 28a000f0 48a00300 e3130004 

I/DEBUG   ( 2066):     401e5148 1491a004 1480a004 e0422003 e2522020 

I/DEBUG   ( 2066):     401e5158 3a000008 e3c1c01f e28cc040 e8b10ff0 

I/DEBUG   ( 2066):

I/DEBUG   ( 2066): code around lr:

I/DEBUG   ( 2066):     401d609c 447b4b13 42b3e010 6a1ed10e 44784811 

I/DEBUG   ( 2066):     401d60ac ec84f7fb ea0ef00d 46224631 efe0f00e 

I/DEBUG   ( 2066):     401d60bc d00a3001 e00b2400 2b00681b 480ad1eb 

I/DEBUG   ( 2066):     401d60cc 44782403 ec72f7fb f001e002 6804fa23 

I/DEBUG   ( 2066):     401d60dc fa20f001 46206005 bf00bd70 0003b306 

I/DEBUG   ( 2066):     401d60ec 0003b2fa 0003b2f2 0003b2ce bf7ef7ff 

I/DEBUG   ( 2066):     401d60fc 4a3e4b3d e92d447b b08b43f0 4606589c 

I/DEBUG   ( 2066):     401d610c 6823460d 930946a1 fa04f001 8000f8d0 

I/DEBUG   ( 2066):     401d611c d0482d00 f0104628 280ff82d d8444604 

I/DEBUG   ( 2066):     401d612c ffe4f7ff d1064286 4629200f e8d8f00d 

I/DEBUG   ( 2066):     401d613c d03c2800 482ee02e f7fb4478 482debb6 

I/DEBUG   ( 2066):     401d614c e0154478 d11342b0 482b6a06 f7fb4478 

I/DEBUG   ( 2066):     401d615c 4a2aec2e 46332120 a801447a fb4ef013 

I/DEBUG   ( 2066):     401d616c a8012101 fe68f01a 46061c42 e011d104 

I/DEBUG   ( 2066):     401d617c 28006800 e02cd1e6 46294630 f00d4622 

I/DEBUG   ( 2066):     401d618c 1c43e914 d11e4607 f9c4f001 29046801 

W/audio_hw_primary( 2070): ret -32, pcm write 768 error wait error: hw 0x12300 app 0x12300 avail 0x0

W/audio_hw_primary( 2070): : Unknown error -32.

I/ServiceManager( 2063): service 'media.audio_policy' died

W/AudioSystem( 2664): AudioPolicyService server died!

I/ServiceManager( 2063): service 'media.audio_flinger' died

I/ServiceManager( 2063): service 'media.player' died

I/BootReceiver( 2451): Copying /data/tombstones/tombstone_01 to DropBox (SYSTEM_TOMBSTONE)

I/ServiceManager( 2063): service 'media.camera' died

W/AudioSystem( 2664): AudioFlinger server died!

W/AudioSystem( 2451): AudioPolicyService server died!

W/AudioSystem( 3221): AudioFlinger server died!

W/IMediaDeathNotifier( 3221): media server died

E/MediaPlayer( 3221): error (100, 0)

W/IMediaDeathNotifier( 2451): media server died

E/MediaPlayer( 3221): error (100, 0)

W/IMediaDeathNotifier( 2500): media server died

E/MediaPlayer( 3221): Error (100,0)

W/AudioSystem( 2451): AudioFlinger server died!

E/MediaPlayer( 3221): Error (100,0)

D/dalvikvm( 2451): GC_FOR_ALLOC freed 119K, 12% free 5979K/6732K, paused 44ms, total 45ms

E/AudioService( 2451): Media server died.

D/dalvikvm( 2451): GC_FOR_ALLOC freed 117K, 13% free 6018K/6864K, paused 35ms, total 35ms

I/dalvikvm-heap( 2451): Grow heap (frag case) to 6.085MB for 131088-byte allocation

D/dalvikvm( 2451): GC_FOR_ALLOC freed <1K, 12% free 6145K/6972K, paused 34ms, total 34ms

D/dalvikvm( 2451): GC_FOR_ALLOC freed <1K, 12% free 6145K/6972K, paused 36ms, total 36ms

I/dalvikvm-heap( 2451): Grow heap (frag case) to 6.272MB for 196628-byte allocation

 

Rock / UIC

Labels (2)
0 Kudos
Reply
1 Reply

1,707 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Rock Lee,

Are you using our SABRE Board, and the Official FSL BSP, and added the CODECS to your image?.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply