iMX536 NVCC_SRTC Abnormal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX536 NVCC_SRTC Abnormal

1,488 次查看
xiaobingtang
Contributor I

     Hello,I come here for your help!   

    
     It is like this: Use LTC3589-1 as a PMIC For iMX536, connet LDO1 to NVCC_SRTC_1V3. When not Powrn ON, the LDO1 out is 1.3V,after power on,LDO1 changes to 1.8V.when I Cut off the connectiong between NVCC_SRTC_1V3 and LTC3589-1's LDO1,NVCC_SRTC_1V3's voltage is 1.8V,and LDO1's voltage is 1.3V.

     Is there something settings wrong?

     PS: LDO power input VDD_REG is measured as 2.5V.

标签 (1)
0 项奖励
回复
1 回复

1,368 次查看
DonnyChiu
Contributor II

Check the following signals in your schematic:

CKIL, ECKIL, PMIC_ON_REQ, PMIC_STBY_REQ.

These signals also use NVCC_SRTC_POW as power source.

Probably, you had one of these signals connected to IC that uses 1.8V level,

and it got leaked to NVCC_SRTC_POW pin.

0 项奖励
回复