iMX53 GPU Tearing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 GPU Tearing

1,520件の閲覧回数
BrianEdmond
Contributor II


Hello,

We are using an iMX53 with OpenGL ES 2.0 and Framebuffer mode, not X11.  When rendering with animation the screen is tearing badly which looks like the display is not actually double buffered.  I am unable to find a setting or option to enable double buffering and was wondering if there is a specific setting required for double buffering or a configuration option of some sort?

Thanks

ラベル(3)
0 件の賞賛
返信
1 返信

1,370件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brian

I am afraid double buffering is not implemented in BSP, one can add

such support using suggestions on

https://community.freescale.com/message/581458#comment-581458

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信