在進入 suspend 模式時, (echo mem > /sys/power/state) ,
為了減少 suspend 的電流,需要對 imx51 的 gpio 作重新設置嗎?
例如:設置為 High-Z (input) mode,以減少電流消耗。
在其他的 application processor 都有類似的動作,但是在 imx51 android bsp 中沒有看到。
請問 imx51 不需要這樣作嗎?
謝謝
Translation: Subject---is it necessary to set GPIO pin to high-Z when entering Suspend mode in i.MX51 Androd 10.4?
When entering suspend mode, in order to reduce current, is it necessary to set GPIO pins? For example, set pin to High-Z (input) mode to reduce power consumption. In other application platform, it is required to do it. However, in i.MX51 bsp, it is not seen.
Does i.MX51 not need the action?
已解决! 转到解答。
Hi Vincent
Do you have 2.6.35 kernel. If so you can refer to arch/arm/mach-mx5/mx50_rdp.c.
There's a suspend enter/exit callback to do such GPIO pin configurations:
static struct mxc_pm_platform_data mx50_pm_data = {
.suspend_enter = mx50_suspend_enter,
.suspend_exit = mx50_suspend_exit,
};
We define a sets of iomux which you want that gpio configured, define all the pins as GPIO like:
static iomux_v3_cfg_t suspend_enter_pads[] = {
MX50_PAD_EIM_DA0__GPIO_1_0,
MX50_PAD_EIM_DA1__GPIO_1_1,
MX50_PAD_EIM_DA2__GPIO_1_2,
MX50_PAD_EIM_DA3__GPIO_1_3,
MX50_PAD_EIM_DA4__GPIO_1_4,
In mx50_suspend_enter callback, we unset the PAD CTRL mask, and save current iomux configuration, set them all to GPIO ALT:
for (i = 0; i < ARRAY_SIZE(suspend_enter_pads); i++) {
suspend_exit_pads[i] = *p;
*p &= ~MUX_PAD_CTRL_MASK;
p++;
}
mxc_iomux_v3_get_multiple_pads(suspend_exit_pads,
ARRAY_SIZE(suspend_exit_pads));
mxc_iomux_v3_setup_multiple_pads(suspend_enter_pads,
ARRAY_SIZE(suspend_enter_pads));
In mx50_suspend_exit callback, restore all the iomux configurations:
mxc_iomux_v3_setup_multiple_pads(suspend_exit_pads,
ARRAY_SIZE(suspend_exit_pads));
vincent_rtk, if your question has been answered, please select Correct Answer so that we can close the DI.
Thanks,
Yixing
Hi Vincent
Do you have 2.6.35 kernel. If so you can refer to arch/arm/mach-mx5/mx50_rdp.c.
There's a suspend enter/exit callback to do such GPIO pin configurations:
static struct mxc_pm_platform_data mx50_pm_data = {
.suspend_enter = mx50_suspend_enter,
.suspend_exit = mx50_suspend_exit,
};
We define a sets of iomux which you want that gpio configured, define all the pins as GPIO like:
static iomux_v3_cfg_t suspend_enter_pads[] = {
MX50_PAD_EIM_DA0__GPIO_1_0,
MX50_PAD_EIM_DA1__GPIO_1_1,
MX50_PAD_EIM_DA2__GPIO_1_2,
MX50_PAD_EIM_DA3__GPIO_1_3,
MX50_PAD_EIM_DA4__GPIO_1_4,
In mx50_suspend_enter callback, we unset the PAD CTRL mask, and save current iomux configuration, set them all to GPIO ALT:
for (i = 0; i < ARRAY_SIZE(suspend_enter_pads); i++) {
suspend_exit_pads[i] = *p;
*p &= ~MUX_PAD_CTRL_MASK;
p++;
}
mxc_iomux_v3_get_multiple_pads(suspend_exit_pads,
ARRAY_SIZE(suspend_exit_pads));
mxc_iomux_v3_setup_multiple_pads(suspend_enter_pads,
ARRAY_SIZE(suspend_enter_pads));
In mx50_suspend_exit callback, restore all the iomux configurations:
mxc_iomux_v3_setup_multiple_pads(suspend_exit_pads,
ARRAY_SIZE(suspend_exit_pads));