iMX287 reset issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX287 reset issue

1,936 Views
___myir
Contributor II

Hi All,

We used iMX287 MCU to design our board, it has dual ETHs.

But if I enable ETHs from kernel, I can't reset the board by press the reset key or run "reboot" command, and if I disable ETHs from kernel, I can reset the board correctly. Are there any conflicts between the chip and the ETHs? or any points we need to attend when design the board?

I would very appreciate any ideas, thanks.

Jakebo

Labels (2)
Tags (2)
2 Replies

1,766 Views
___myir
Contributor II

Hi All,

We got the solution about that, the power of ETHS can't connect to VDDIO, use an extend 3.3v instead.

0 Kudos
Reply

1,766 Views
gusarambula
NXP TechSupport
NXP TechSupport

I’m glad to hear you got to fix your problem and thank you for posting the solution as this will help other users that find similar issues. The ENETs probably drained more current than what the VDDIO could supply from a PMU perspective, for more information please refer to the PMU section of the i.MX28 Datasheet.

0 Kudos
Reply