iMX286 Current Consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX286 Current Consumption

1,715件の閲覧回数
senthilkumarsri
Contributor I

Hi,

In one of our product, we have a processor module which has iMX286 processor, DDR2 SDRAM and NAND memory. The input voltage to this board is 5V and the DDR, NAND are supplied from internal DCDC regulators. I have held the processor RESET and measured the current. It consumes 12mA which i believe is too high. Please clarify.

I have also tried find out the standby current of iMX286, but couldn't find it in any of the document. Could you please let me know the details of standby current.

Regards,
Senthilkumar

ラベル(1)
0 件の賞賛
返信
1 返信

1,613件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Senthilkumar,

Here´s the using i.MX28 power management,

http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf

Regard

0 件の賞賛
返信