iMX28-x-windows problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28-x-windows problems

1,013 Views
Nico
Contributor II

Hi...
i'm working with an imx28 freescale microprocessor and i work with tftp and nfs. I've installed ltib with imx28 configuration..i'm using the freesclae kernel demo.

The kernel go on and the filesystem the same...i come to the loginand after i write "startx" and the answer is:
XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6
_XSERVTransOpen: transport open failed for inet6/freescale:0
_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device Virtual core keyboard
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device (unnamed keyboard)

some suggests??

Thank you..

Labels (1)
0 Kudos
Reply
0 Replies