iMX28 linux 6.6 kernel USB disconnecting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28 linux 6.6 kernel USB disconnecting

846件の閲覧回数
FAlexander
Contributor I

I have enabled

CONFIG_USB_OTG

 CONFIG_USB_OTG_FSM 

CONFIG_USB_EHCI_FSL 

CONFIG_USB_EHCI_HCD_PLATFORM

in linux menuconfig. With this I am able to detect my usb but after bootup it is continuously disconnecting and connecting multiple times. once I adjust the USB to particular position it connects properly. I taught it is a hardware issue but the same board and OTG cable with kernal 2.6 I am not facing this issue.

0 件の賞賛
返信
1 返信

827件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This issue could be caused in porting process since we do not have an official BSP for i.MX28 with 6.6 Kernel.

Best regards.

0 件の賞賛
返信