iMX28 linux 6.6 kernel USB disconnecting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 linux 6.6 kernel USB disconnecting

834 Views
FAlexander
Contributor I

I have enabled

CONFIG_USB_OTG

 CONFIG_USB_OTG_FSM 

CONFIG_USB_EHCI_FSL 

CONFIG_USB_EHCI_HCD_PLATFORM

in linux menuconfig. With this I am able to detect my usb but after bootup it is continuously disconnecting and connecting multiple times. once I adjust the USB to particular position it connects properly. I taught it is a hardware issue but the same board and OTG cable with kernal 2.6 I am not facing this issue.

0 Kudos
Reply
1 Reply

815 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This issue could be caused in porting process since we do not have an official BSP for i.MX28 with 6.6 Kernel.

Best regards.

0 Kudos
Reply