iMX28 Has anyone made a package of the bootstream?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 Has anyone made a package of the bootstream?

1,114 Views
colinmoloney
Contributor II

We are working with the iMX28 with Yocto (morty) building the 4.1 kernel and using the linux.sb & linux.sdcard output to burn a µSD image.  We use rpm packages to do over-the-air updates to are target device but the bootstream is not packaged by morty.  I can arrange for the bootstream to be left in "tmp/deploy/images/<machine>" but I don't know how to get the packaging system to make a package of it, preferably named with the same version number as the kernel and it's modules.

Has anyone done this?

0 Kudos
Reply
1 Reply

1,069 Views
art
NXP Employee
NXP Employee

Since the bootstream is the binary monolitic file that contains the initial hardware configuration section, the bootloader and the kernel code, there is no way to make a rpm package of it.

Best Regards,
Artur

0 Kudos
Reply