iMX25 DDR2 layout inquiry:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX25 DDR2 layout inquiry:

1,497 次查看
yuanli
NXP Employee
NXP Employee

on our old iMX25 board(6-layer through whole board), there are 27ohm resistors between iMX25 and DDR2. Are these resistors necessary? can we remove them, our new board size is much smaller? Another question is could we change the DDR2 DATA lines connection order by group? thanks.

标签 (1)
0 项奖励
回复
1 回复

1,331 次查看
Yuri
NXP Employee
NXP Employee

Basically, the best approach - to use simulation technique for PCB design.

In the same time, general rules may be provided for customers to simplify their

PCB considerations, but note, for assurance such rules are very strong.

  So, if You can simulate the PCB design please use it, if cannot - please follow

general (and more strong) recommendations. To avoid signal overshooting, please

try to apply different drive strength options for both i.MX25 and DDR2 part. In particular,

section 1.3 (Calculating the Characteristic Impedance) of app note AN3963 shows how to

estimate it. Also one can apply to JEDEC recommendations for DIMM / SODIMM (termination)

schemes.

  Finally, please refer to section 3 (mDDR and DDR2 Routing Guidelines) of AN4017.

Below are app note links :

http://cache.freescale.com/files/dsp/doc/app_note/AN3963.pdf

http://cache.freescale.com/files/dsp/doc/app_note/AN4017.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------