iMX RT1064 | PowerCore VCC_SOC_IN (1-9 pins)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1064 | PowerCore VCC_SOC_IN (1-9 pins)

931 Views
shai_b
Senior Contributor II

Hi Team,

My customer would like to know if there is any need to connect the VCC_SOC_IN to any inputs or these pins are internally connected to the Core?

Secondly, regards the ON/OFF Pin, once the device gets power-on in case the pin is on ON the device will startup or there is a need to wake up the device?

Thanks in advance 

KR,

Shai

Labels (1)
0 Kudos
Reply
3 Replies

926 Views
Yuri
NXP Employee
NXP Employee

@shai_b 
Hello,

 1. 
     It is highly recommended to connect ALL VCC_SOC_IN pins to external power supply.

2.
   ON/OFF behavior is described as following:

  A brief connection to GND in the OFF mode causes the internal power management
state machine to change the state to ON. In the ON mode, a brief connection to GND
generates an interrupt (intended to be a software-controllable power-down).
Approximately five seconds (or more) to GND causes a forced OFF

Regards,
Yuri.

0 Kudos
Reply

923 Views
shai_b
Senior Contributor II

Hi @Yuri,

Thanks a lot for your inputs, I want just to get confirmation from your side

as I understand if my customer would like to use our RT1064 MCU on battery it is best to use an external DC/DC power supply (1.2v) for all ALL VCC_SOC_IN pins?

in addition, what is the current consumption is needed for powering the Core? and if there is any suggestion for battery operation with the RT family?

Thanks in advance 

KR,

Shai 

 

0 Kudos
Reply

920 Views
Yuri
NXP Employee
NXP Employee

@shai_b 
 

   Follow the reference design (DCDC_OUT is connected with VDD_SOC_IN).
For power consumption, please refer to the following app note:

"Power Consumption and Measurement of i.MXRT1060"

https://www.nxp.com/docs/en/application-note/AN12245.pdf

 

~Yuri.

0 Kudos
Reply