Hello,
The decision XIP or not is based on the used addresses (which may be found in the IVT).
For XIP boot, the image has to be built for FlexSPI address space and for non XIP the image
can be built to execute from Internal RAM. Basically any memory may be used for non-XIP
approach, but external memory should be init before using via the DCD.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------