i2c sending failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i2c sending failed

6,820件の閲覧回数
PramodKumar
Contributor IV

hii

i am using 2.6.35.3 kernel in ltib but when i want used the i2c device its like rtc and tcp ip its producing "Failed writing to the I2C-bus: Connection timed out  "

example:

[root@alarm i2c]# ./i2c-tool -w 0 0x48 4 0x02 0xA0 0x40 0x03              
SLAVE ADDRESS: 0x48                                                       
NUMBER OF BYTES TO WRITE: 4                                               
MEMORY ALLOCATED AT ADDRESS: 0x12008                                      
/dev/i2c-0 OPENDED!                                                       
Failed writing to the I2C-bus: Connection timed out                                                                        

Thanks&regard

pramod kumar

ラベル(5)
0 件の賞賛
返信
6 返答(返信)

5,112件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

before writing, file /dev/i2c-0 should be created manually, please look

at correct procedure below

All Boards I2C-tools

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,112件の閲覧回数
PramodKumar
Contributor IV

Hii

  Thanks for that ..i have followed  all process also uesd I2C-tool but when run this command it s producing this ..and i am working on imx233 board

plz tell me how to solve this problem

root@freescale /home$ i2cdetect -l

i2c-0   i2c             MXS I2C adapter                         I2C adapter

root@freescale /home$ i2cdetect 0

WARNING! This program can confuse your I2C bus, cause data loss and worse!     

I will probe file /dev/i2c-0.                                                  

I will probe address range 0x03-0x77.                                          

Continue? [Y/n] y                                                              

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f                            

00:          -- -- -- -- -- -- -- -- -- -- -- -- --hw_i2c_dma_setup_read       

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --                            

20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --                            

30: ��-- hw_i2c_dma_setup_read��-- hw_i2c_dma_setup_read                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- -- -- -- -- -- -- -- --                                                     

40: -- -- -- -- -- -- -- -- -- -- hw_i2c_dma_setup_read-- -- -- -- -- --       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

-- hw_i2c_dma_setup_read                                                       

--                                                                             

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --                            

70: -- -- -- -- -- -- -- --

....................................................................................................................................................................................................................    

root@freescale /home$ i2cdump 0 0x6a  

No size specified (using byte-data access)

WARNING! This program can confuse your I2C bus, cause data loss and worse!

I will probe file /dev/i2c-0, address 0x6a, mode byte

Continue? [Y/n] y

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef

XX XX XX XX X� XX XX XX XX XX XXXXXXXXXXXXXXXXXX
10: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
20: XX XX XX XX XX XX XX XX XX XX .�Minicom2.5XX XX XX XX XXXXXXXXXXXXXXXXXX
30: XX XX XX XX XX XX XX .�Minicom2.5X XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
40: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
50: XX XX .�Minicom2.5XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
60: XX XX XX XX XX XX XX XX XX XX XX .�Minicom2.5XX XX XX XXXXXXXXXXXXXXXXXX
70: XX X�Minicom2.5XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
80: XX .�Minicom2.5XX XX XX XX XX XX .�Minicom2.5XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX
90: XX XX XX XX X�Minicom2.5XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXXXX

a0: XX .�Minicom2.5XX XX XX XX .�Minicom2.5XX XX .�Minicom2.5.�Minicom2.5XX XX XX XX ....XXXXXXXXXXXXXXXX

b0: Minicom2.5XX XX XX XX XX .�Minicom2.5XX XX XX XX XX

......................................................................................................................................................................................................................

root@freescale /home$  i2cset 0 0x6a 01 0x0008 w

WARNING! This program can confuse your I2C bus, cause data loss and worse!

I will write to device file /dev/i2c-0, chip address 0x6a, data address

0x01, data 0x08, mode word.

Continue? [Y/n] y

Error: Write failed

0 件の賞賛
返信

5,112件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

please try latest official i.MX23 EVK Linux BSP release

L2.6.31_10.05.00_SDK_SOURCE  : Linux 2.6.31 Source Code Files 2010.05 Release.

~igor

0 件の賞賛
返信

5,112件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Hi Pramod,

I suggest you to use kernel 4.1 with and apply the following patch:

https://git.kernel.org/cgit/linux/kernel/git/shawnguo/linux.git/commit/arch/arm/boot/dts/imx23.dtsi?...

It will be part of 4.2 kernel, but you can apply it manually and I2C will work. Then you can add the dts entry in the imx23-olinuxino device tree file.

Regards,

Fabio Estevam

0 件の賞賛
返信

5,112件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
0 件の賞賛
返信

5,112件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

if you are using successfully imx233-olimax kernel,

then seems your board is based on olimax board.

Suggested Linux BSP release was developed for i.MX23 EVK,

not for olimax board. I would suggest to post this to

Olimex

~igor

0 件の賞賛
返信