i used iMX6 CPU, could you tell me

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i used iMX6 CPU, could you tell me

820 Views
tintai
Contributor I

Dear,

i used iMX6 CPU, could you tell me:

1.why DISP0_CLK (PIN86) dcreased to below 2.8V? when Ambient temperature high.

2.why the CPU can not restart?

3.how to solve above 2 problems?

 

                                                     tin tai

0 Kudos
Reply
3 Replies

799 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I need more information about your testing setup.

Are you using a custom board?

Did you do a DDR stress test? 

Which OS are you using?

How can I reproduce the issue in my side?

Best regards.

 

741 Views
tintai
Contributor I

dear JorgeCas

i use MCIMX6D6AVT10AD.

sorry, i can not tell you testing setup.

Are you using a custom board? no

Did you do a DDR stress test? no

can you answer my questions by theory?

0 Kudos
Reply

729 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

To ensure we can provide you with the most effective support, it would be very helpful if you could share the details of your setup. Without that information, it’s much more challenging to diagnose the issue accurately.

Since you are no using a custom board, if you are using our pre-built BSP you should can reset your board without any problem.

If you are using a custom image, please check the changes you did in the image.

Best regards.