i.mx8m plus 12 bit grayscale camera iterface issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m plus 12 bit grayscale camera iterface issue

6,396 Views
tdave
Contributor I

Hello,

We are trying to interface a 3rd party camera sensor configured for12 bit grayscale output with resolution of 640x480. However when trying to capture the raw image through v4l2-ctl, we are not seeing expected data in the captured frame.

We made changes suggested in https://community.nxp.com/t5/i-MX-Processors/How-to-set-up-the-MIPI-CSI-2-and-ISI-to-transfer-RAW10-.... However we are still not seeing a valid camera output through v4l2-ctl.

Below are the changes that we have made

Added the below format to mxc_isi_src_formats[]

 

{
	.name		= "Y12 (Grey)",
	.fourcc		= V4L2_PIX_FMT_Y12,
	.depth		= { 12 },
	.memplanes	= 1,
	.colplanes	= 1,
	.align		= 1,
}
struct mxc_isi_fmt *mxc_isi_get_src_fmt(struct v4l2_subdev_format *sd_fmt)
 	sd_fmt->format.code == MEDIA_BUS_FMT_UYVY8_2X8 ||
 	sd_fmt->format.code == MEDIA_BUS_FMT_YUYV8_2X8)
 	    index = 1;
+	else if (sd_fmt->format.code == MEDIA_BUS_FMT_Y12_1X12)
+	    index = 2;
 	else
 	    index = 0;

 

 

Added below format to mxc_isi_out_formats[]

 

 {
	.name		= "Y12",
	.fourcc		= V4L2_PIX_FMT_Y12,
	.depth		= { 12 },
	.color		= MXC_ISI_OUT_FMT_RAW12,
	.memplanes	= 1,
	.colplanes	= 1,
	.align		= 1,
	.mbus_code	= MEDIA_BUS_FMT_Y12_1X12,
}

 

 

Set the ISI CSC in bypass mode:

 

	// if (is_yuv(src_fmt->fourcc) && is_rgb(dst_fmt->fourcc)) {
	// 	/* YUV2RGB */
	// 	csc = YUV2RGB;
	// 	/* YCbCr enable???  */
	// 	val |= (CHNL_IMG_CTRL_CSC_MODE_YCBCR2RGB << CHNL_IMG_CTRL_CSC_MODE_OFFSET);
	// 	val |= (CHNL_IMG_CTRL_YCBCR_MODE_ENABLE << CHNL_IMG_CTRL_YCBCR_MODE_OFFSET);
	// } else if (is_rgb(src_fmt->fourcc) && is_yuv(dst_fmt->fourcc)) {
	// 	/* RGB2YUV */
	// 	csc = RGB2YUV;
	// 	val |= (CHNL_IMG_CTRL_CSC_MODE_RGB2YCBCR << CHNL_IMG_CTRL_CSC_MODE_OFFSET);
	// } else {
	// 	/* Bypass CSC */
 		pr_info("bypass csc\n");
 		mxc_isi->cscen = 0;
 		val |= CHNL_IMG_CTRL_CSC_BYPASS_ENABLE;

 

 

Add the Y12 format to imx8-mipi-csi2-sam.c

 

static int csis_s_fmt(struct v4l2_subdev *sd, struct csi_sam_format *fmt)
 	case V4L2_PIX_FMT_SRGGB12:
 	    code = MEDIA_BUS_FMT_SRGGB12_1X12;
 	    break;
+	case V4L2_PIX_FMT_Y12:
+	    code = MEDIA_BUS_FMT_Y12_1X12;
+	    break;
 	default:
 		return -EINVAL;

 

 
v4l2-ctl command to capture the camera frame:

 

v4l2-ctl --verbose --device /dev/video2 --stream-mmap --stream-to=frame.raw --stream-count=1 --set-fmt-video=width=640,height=480,pixelformat='Y12 '

 


ISI register dump during the capture:

[   38.142066] mxc-isi 32e00000.isi: ISI CHNLC register dump, isi0
[   38.148041] mxc-isi 32e00000.isi:            CHNL_CTRL[0x00]: e0000000
[   38.154595] mxc-isi 32e00000.isi:        CHNL_IMG_CTRL[0x04]: e000001
[   38.161123] mxc-isi 32e00000.isi:    CHNL_OUT_BUF_CTRL[0x08]: 7c707
[   38.167415] mxc-isi 32e00000.isi:         CHNL_IMG_CFG[0x0c]: 1e00280
[   38.173874] mxc-isi 32e00000.isi:             CHNL_IER[0x10]: 3cfc0000
[   38.180420] mxc-isi 32e00000.isi:             CHNL_STS[0x14]: 100
[   38.186540] mxc-isi 32e00000.isi:    CHNL_SCALE_FACTOR[0x18]: 10001000
[   38.193090] mxc-isi 32e00000.isi:    CHNL_SCALE_OFFSET[0x1c]: 00
[   38.199115] mxc-isi 32e00000.isi:        CHNL_CROP_ULC[0x20]: 00
[   38.205142] mxc-isi 32e00000.isi:        CHNL_CROP_LRC[0x24]: 00
[   38.211169] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF0[0x28]: 00
[   38.217198] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF1[0x2c]: 00
[   38.223222] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF2[0x30]: 00
[   38.229249] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF3[0x34]: 00
[   38.235274] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF4[0x38]: 00
[   38.241302] mxc-isi 32e00000.isi:      CHNL_CSC_COEFF5[0x3c]: 00
[   38.247325] mxc-isi 32e00000.isi:     CHNL_ROI_0_ALPHA[0x40]: 00
[   38.253351] mxc-isi 32e00000.isi:       CHNL_ROI_0_ULC[0x44]: 00
[   38.259378] mxc-isi 32e00000.isi:       CHNL_ROI_0_LRC[0x48]: 00
[   38.265412] mxc-isi 32e00000.isi:     CHNL_ROI_1_ALPHA[0x4c]: 00
[   38.271440] mxc-isi 32e00000.isi:       CHNL_ROI_1_ULC[0x50]: 00
[   38.277465] mxc-isi 32e00000.isi:       CHNL_ROI_1_LRC[0x54]: 00
[   38.283491] mxc-isi 32e00000.isi:     CHNL_ROI_2_ALPHA[0x58]: 00
[   38.289514] mxc-isi 32e00000.isi:       CHNL_ROI_2_ULC[0x5c]: 00
[   38.295541] mxc-isi 32e00000.isi:       CHNL_ROI_2_LRC[0x60]: 00
[   38.301587] mxc-isi 32e00000.isi:     CHNL_ROI_3_ALPHA[0x64]: 00
[   38.307627] mxc-isi 32e00000.isi:       CHNL_ROI_3_ULC[0x68]: 00
[   38.313655] mxc-isi 32e00000.isi:       CHNL_ROI_3_LRC[0x6c]: 00
[   38.319683] mxc-isi 32e00000.isi: CHNL_OUT_BUF1_ADDR_Y[0x70]: 84500000
[   38.326251] mxc-isi 32e00000.isi: CHNL_OUT_BUF1_ADDR_U[0x74]: 00
[   38.332288] mxc-isi 32e00000.isi: CHNL_OUT_BUF1_ADDR_V[0x78]: 00
[   38.338323] mxc-isi 32e00000.isi:   CHNL_OUT_BUF_PITCH[0x7c]: 3c0
[   38.344437] mxc-isi 32e00000.isi:     CHNL_IN_BUF_ADDR[0x80]: 00
[   38.350482] mxc-isi 32e00000.isi:    CHNL_IN_BUF_PITCH[0x84]: 00
[   38.356517] mxc-isi 32e00000.isi:     CHNL_MEM_RD_CTRL[0x88]: 00
[   38.362569] mxc-isi 32e00000.isi: CHNL_OUT_BUF2_ADDR_Y[0x8c]: 84100000
[   38.369122] mxc-isi 32e00000.isi: CHNL_OUT_BUF2_ADDR_U[0x90]: 00
[   38.375149] mxc-isi 32e00000.isi: CHNL_OUT_BUF2_ADDR_V[0x94]: 00
[   38.381177] mxc-isi 32e00000.isi:     CHNL_SCL_IMG_CFG[0x98]: 1e00280
[   38.387638] mxc-isi 32e00000.isi:       CHNL_FLOW_CTRL[0x9c]: 00

dmesg logs showing camera driver linking to mipi and isi

 

[    8.149343] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[    8.157345] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[    8.181549] mx8-img-md: created link [test_cameras 0-0030] => [mxc-mipi-csi2.0]

 


We would appreciate any help or suggestion to resolve this issue.

Thanks,
Tareesh

Labels (1)
0 Kudos
Reply
10 Replies

6,357 Views
joanxie
NXP TechSupport
NXP TechSupport

since imx8mp has ISP which can support raw data directly, why do you need to use ISI? do you want to get rgb output?

0 Kudos
Reply

6,346 Views
tdave
Contributor I

Hello @joanxie , Thank you for your response.

We are using ISI with our other camera which uses YUV 4:2:0 format and we wanted to keep the same interface for this other camera sensor. Is the raw mode not supported through ISI ? If we have to switch to using ISP, is there any documentation/guide I can refer to?

Thanks,
Tareesh

0 Kudos
Reply

6,335 Views
joanxie
NXP TechSupport
NXP TechSupport

ISI can support raw data, but couldn't handle this, if you want to use ISI, it's ok, I checked your source code, I think this should be 16

.depth		= { 12 },
0 Kudos
Reply

6,325 Views
tdave
Contributor I

Hello @joanxie ,

I implemented the change to depth as you suggested but still don't see a valid frame.

.name		= "Y12 (Grey)",
.fourcc		= V4L2_PIX_FMT_Y12,
.depth		= { 16 },
.memplanes	= 1,
.colplanes	= 1,
.align		= 1,
.name		= "Y12",
.fourcc		= V4L2_PIX_FMT_Y12,
.depth		= { 16 },
.color		= MXC_ISI_OUT_FMT_RAW12,
.memplanes	= 1,
.colplanes	= 1,
.align		= 1,
.mbus_code	= MEDIA_BUS_FMT_Y12_1X12,

 

Once I tested the depth change, I also made the following changes to imx8-mipi-csi2-sam.c

static const struct csis_pix_format mipi_csis_formats[]
+{
+	.code = MEDIA_BUS_FMT_Y12_1X12,
+	.fmt_reg = MIPI_CSIS_ISPCFG_FMT_RAW12,
+	.data_alignment = 16,
+},

static void disp_mix_gasket_config(struct csi_state *state)
+ case MEDIA_BUS_FMT_Y12_1X12:
+	fmt_val = GASKET_0_CTRL_DATA_TYPE_RAW12;
+	break;

static int csis_s_fmt(struct v4l2_subdev *sd, struct csi_sam_format *fmt)
+ case V4L2_PIX_FMT_Y12:
+    code = MEDIA_BUS_FMT_Y12_1X12;
+    break;

But still no luck with capturing a valid frame

Here is the v4l2-ctl output:

root@test~# v4l2-ctl --verbose --device /dev/video2 --stream-mmap --stream-to=frame.raw --stream-count=1 --set-fmt-video=width=640,height=480,pixelformat='Y12 '
VIDIOC_QUERYCAP: ok
VIDIOC_G_FMT: ok
VIDIOC_S_FMT: ok
Format Video Capture Multiplanar:
        Width/Height      : 640/480
        Pixel Format      : 'Y12 ' (12-bit Greyscale)
        Field             : None
        Number of planes  : 1
        Flags             :
        Colorspace        : Raw
        Transfer Function : Default
        YCbCr/HSV Encoding: ITU-R 601
        Quantization      : Full Range
        Plane 0           :
           Bytes per Line : 1280
           Size Image     : 614400
                VIDIOC_REQBUFS returned 0 (Success)
                VIDIOC_QUERYBUF returned 0 (Success)
                VIDIOC_QUERYBUF returned 0 (Success)
                VIDIOC_QUERYBUF returned 0 (Success)
                VIDIOC_QUERYBUF returned 0 (Success)
                VIDIOC_QBUF returned 0 (Success)
                VIDIOC_QBUF returned 0 (Success)
                VIDIOC_QBUF returned 0 (Success)
                VIDIOC_QBUF returned 0 (Success)
                VIDIOC_STREAMON returned 0 (Success)
cap dqbuf: 0 seq:      1 bytesused: 614400 ts: 33.186146 (ts-monotonic, ts-src-eof)

 

0 Kudos
Reply

6,296 Views
tdave
Contributor I

Dump of MIPI CSI2 registers:

[  452.436044] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[  452.441362] mxc-mipi-csi2.0:         CSIS_VERSION[0]: 0x03060301
[  452.447413] mxc-mipi-csi2.0:        CSIS_CMN_CTRL[4]: 0x00004905
[  452.453459] mxc-mipi-csi2.0:        CSIS_CLK_CTRL[8]: 0x000f0000
[  452.459509] mxc-mipi-csi2.0:          CSIS_INTMSK[10]: 0x0fffff1f
[  452.465708] mxc-mipi-csi2.0:          CSIS_INTSRC[14]: 0x00000000
[  452.471832] mxc-mipi-csi2.0:      CSIS_DPHYSTATUS[20]: 0x000000f1
[  452.477950] mxc-mipi-csi2.0:        CSIS_DPHYCTRL[24]: 0x0d800007
[  452.484064] mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_L[30]: 0x000001f4
[  452.490175] mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_H[34]: 0x00000000
[  452.496288] mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_L[38]: 0x00000000
[  452.502402] mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_H[3c]: 0x00000000
[  452.508513] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH0[40]: 0x000000b0
[  452.514627] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH1[50]: 0x000008fd
[  452.520734] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH2[60]: 0x000008fe
[  452.526843] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH3[70]: 0x000008ff
[  452.532951] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH0[44]: 0x01e00280
[  452.539061] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH1[54]: 0x80008000
[  452.545169] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH2[64]: 0x80008000
[  452.551281] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH3[74]: 0x80008000
[  452.557390] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH0[48]: 0x00000000
[  452.563507] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH1[58]: 0x00000000
[  452.569622] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH2[68]: 0x00000000
[  452.575752] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH3[78]: 0x00000000
[  452.581875] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[  452.587122] mxc-mipi-csi2.0:    GPR_GASKET_0_CTRL[60]: 0xffff8000
[  452.593240] mxc-mipi-csi2.0:   GPR_GASKET_0_HSIZE[64]: 0xffff8000
[  452.599352] mxc-mipi-csi2.0:   GPR_GASKET_0_VSIZE[68]: 0xffff8000
0 Kudos
Reply

6,290 Views
joanxie
NXP TechSupport
NXP TechSupport

你可以参考下下面两个客户的配置,我这里没有raw12的camera可以复现这个问题,首先可以看下你的camera 是什么模式,连续还是非连续的,我看这个客户depth用12也可以成功捕获图像

“https://community.nxp.com/t5/i-MX-Processors/raw12-camera-on-imx8mp-isi/m-p/1653019”

“https://community.nxp.com/t5/i-MX-Processors/imx8mp-Failed-to-obtain-sensor-raw12-data/m-p/1537266”

 

0 Kudos
Reply

6,245 Views
tdave
Contributor I

After enabling the debug logs for the MIPI interrupts, I noticed the following in the logs:

[  475.813567] mxc-mipi-csi2.0: SOT Error: 1
[  475.817582] mxc-mipi-csi2.0: Lost Frame Start Error: 1
[  475.822723] mxc-mipi-csi2.0: status: 00031000

 

We have the following values in the device tree:

data-lanes = <2>;
csis-hs-settle = <13>;
csis-clk-settle = <2>;

 

@joanxie I would appreciate if you could give some suggestion as to what might be wrong in the configuration to cause the start of frame to be lost.

Thanks.

 

0 Kudos
Reply

6,224 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems that the timing issue, you can refer to the chapter 3.2.5 DPHY high-speed settle timer of enclosed file

0 Kudos
Reply

6,151 Views
tdave
Contributor I

I have set the value based on the document. But still don't see any valid frame output.

csis-hs-settle = <17>;
csis-clk-settle = <2>;

Thanks,
Tareesh

Tags (1)
0 Kudos
Reply

6,113 Views
joanxie
NXP TechSupport
NXP TechSupport

did you set this based on your measured clock by Oscilloscope? if no, try to measure it

0 Kudos
Reply