i.mx8 Fuse map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8 Fuse map

2,585件の閲覧回数
mobrien
Contributor II

Thanks Shivani and Yuri,

Is there a unique ID in the fusemap that we can read?

Also - can we use the _GP registers listed on page 850 of the RM: HCOTP_HW_OCOTP_GP10 etc to store some data specificaly for our software?

Also - I'm finding that the addressing from the blog link above is not working with the version of uboot that I have.

=> fuse prog 0 708 0xa295fc11

Best Regards,

-Mike

0 件の賞賛
返信
1 返信

2,516件の閲覧回数
Yuri
NXP Employee
NXP Employee

[email protected] 

Hello,

  i.MX8M RM contains fusemap chapter, in particular in Table 6-43 (Fusemap Descriptions)
of i.MX 8M Dual/8M QuadLite/8M Quad  Reference Manual, Rev. 2, 08/2019, UNIQUE_ID
fuse is located in Fuse Address offsets (0x410 and) 0x420. To get the values -
read the bank 0, words 1 and 2.

fuse read 0 1
fuse read 0 2

  As for the General Purpose fuse registers - some of them are reserved, in any case we cannot

not guarantee them for free using.

Regards,

Yuri.

0 件の賞賛
返信