i.mx6ul wakeup source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6ul wakeup source

1,607件の閲覧回数
strive
Contributor I

Dear  Expert:

i.mx6ul has lots of wakeup source,such as gpio,rtc,CAN,etc.

Is there a method to know which wakeup source wakes up the i.mx6ul  when  i.mx6ul is waked up from sleep,such as through some registers?

thanks for your support.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,443件の閲覧回数
strive
Contributor I

thanks for your support.

Furthermore, could you tell me which register reflect this?

0 件の賞賛
返信

1,443件の閲覧回数
b36401
NXP Employee
NXP Employee

You can perform the command like "dmidecode | grep -i wake".

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信