i.mx6ul wakeup source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6ul wakeup source

1,622 Views
strive
Contributor I

Dear  Expert:

i.mx6ul has lots of wakeup source,such as gpio,rtc,CAN,etc.

Is there a method to know which wakeup source wakes up the i.mx6ul  when  i.mx6ul is waked up from sleep,such as through some registers?

thanks for your support.

Labels (1)
0 Kudos
Reply
2 Replies

1,458 Views
strive
Contributor I

thanks for your support.

Furthermore, could you tell me which register reflect this?

0 Kudos
Reply

1,458 Views
b36401
NXP Employee
NXP Employee

You can perform the command like "dmidecode | grep -i wake".

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply