i.mx6q sabresd_6dq simcom 4g module debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6q sabresd_6dq simcom 4g module debug

4,013 Views
blackhuang
Contributor I

Dear NXP fae

                  我正在使用I.MX6Q调试simcom  4g lte module有以下疑问,还请贵司帮助解决一下,

环境:i.mx6q sabresd_6dq    android6.0.1     kernel  4.1.15

module:sim7600

根据simcom的指导文档、我已使用adb方式调试成功。但是该方式在量产时不太方便。

现在想请教的是如何将simcom需要adb进去的库等通过编译到系统中,如:

adb push init.gprs-pppd /etc/
adb push 3gdata_call.conf /etc/
adb shell chmod 777 /etc/init.gprs-pppd

adb push rild /system/bin/
adb shell chmod 777 /system/bin/rild
adb push libreference-ril.so /system/lib/
adb push libril.so /system/lib/

这些文件该如何替换,那些文件可不必替换,直接使用开发板的。

希望得到你们的帮助,十分感谢!!!

0 Kudos
Reply
3 Replies

3,809 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Black,

 See steps below, and try:

(1) Compliling android source code

(2) Copy init.gprs-pppd  to /out/target/..../system/etc (编译输出路径中,输出system.img的地方)

(3)Copy 3gdata_call.conf to /out/target/..../system/etc

(4)Copy rild to /out/target/..../system/bin

(5)Copy libreference-ril.so /out/target/.... /system/lib/

(6)Copy libril.so /out/target/.... /system/lib/

/* the following to lines should added to /out/target/...../init.rc or init.freescale.rc */

(7) chmod 777 /etc/init.gprs-pppd

(8)chmod 777 /system/bin/rild

Then run "make" command, new sysmtem.img will be created.

Have a nice day!

BR,

Weidong

0 Kudos
Reply

3,809 Views
blackhuang
Contributor I

Hi weidong,

                  非常感谢您的帮助,simcom的模块已经完全可以正常工作啦。

出于相关原因,我这边又调试了YUGA的CLM920_EC5模块。在系统中虚拟口ttyUSB可识别。

YUGA的模块只需要更换libreference-ril.so就行。使用系统中自带的rild服务无法识别到模块。修改android/hardware/ril/rild/rild.c 中去掉 //  switchUser();函数和android/hardware/ril/rild/runtime-ril-port/runtime-ril-port.c  增加YUGA模块文件重新生产的rild还是无法正常工作。窗口中一直显示

init: Starting service 'ril-daemon'...
init: Service 'ril-daemon' (pid 4243) killed by signal 4
init: Service 'ril-daemon' (pid 4243) killing any children in process group

 

与YUGA联调,那边工程师反应说是我这边系统的问题。您那边方便给点意见吗?

非常感谢您的帮助。

0 Kudos
Reply

3,809 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Black,

   re-create  a new case for your new question, please!

Have a nice day!

BR,

weidong

0 Kudos
Reply