i.mx6q hangs at Starting kernel log daemon...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6q hangs at Starting kernel log daemon...

3,736 次查看
shijunzhao
Contributor III

The hardware is i.mx6q sabresd board. 

The rootfs I'm using is fsl-image-qt5-validation-imx-fb-imx6qdlsolo in L4.1.15_2.0.0-ga_images_MX6QDLSOLO, and I don't modify the rootfs.

The Linux version is imx_4.1.15_2.0.0_ga.

The rootfs is mounted through NFS.

When I boot the board, it hangs on Starting kernel log daemon... for a long time (about several minutes), and then it hands at umount: /mnt/.psplash: umount failed: No such file or directory. The print log is:

.........

/etc/network/if-pre-up.d/nfsroot: line 12: /proc/mounts: No such file or directory
run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1
Starting system message bus: Failed to start message bus: Failed to bind socket "/var/run/dbus/system_bus_socket": No such file or directory
dbus.
/etc/rc5.d/S05connman: line 15: /proc/mounts: No such file or directory
/etc/rc5.d/S10dropbear: line 32: /proc/mounts: No such file or directory
Starting Dropbear SSH server: dropbear.
Starting rpcbind daemon...done.
starting statd: done
Starting advanced power management daemon: No APM support in kernel
(failed.)
Starting atd: OK
exportfs: can't open /etc/exports for reading
grep: /proc/filesystems: No such file or directory
NFS daemon support not enabled in kernel
Starting system log daemon...0
Starting kernel log daemon...
* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon [fail]
Starting Telephony daemon
Starting Linux NFC daemon
Failed to connect to socket /var/run/dbus/system_bus_socket: No such file or directory
Starting crond: OK
Running local boot scripts (/etc/rc.local)/etc/rc.local: line 15: /proc/sys/vm/min_free_kbytes: No such file or directory
error
umount: /mnt/.psplash: umount failed: No such file or directory

标签 (3)
0 项奖励
回复
3 回复数

2,896 次查看
joanxie
NXP TechSupport
NXP TechSupport

try to use the command :

sudo chmod 777 -R <your Yocto work folder>/fsl-image-qt5/1.0-r0/rootfs, then try build again.

0 项奖励
回复

2,896 次查看
shijunzhao
Contributor III

I don't find your path. I'm using following build commands:

$MACHINE=imx6qsabresd DISTRO=fsl-imx-x11 source ./fsl-setup-release.sh -b bld-x11

$bitbake fsl-image-gui

0 项奖励
回复

2,896 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you use x11 image, you can find your "work" folder under build_x11/tmp/work, can you find it? then find the "rootfs" folder under work/imx6xxx(board name)/fsl-image-gui/1.0-r.0/rootfs

if you can find this folder, try to use the command as I mentioned last time, change the path to your own path. then build again.

0 项奖励
回复