i.mx6 yocto and qt5 Version question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 yocto and qt5 Version question

1,154 Views
kangmw086
Contributor III

I installed the YOCTO GATESGARTH.

GATESGATH created the QT5.15.0 toolchain.

Is there no problem with version compatibility if I install the QT5.14 version on UBUNTU and use it by setting SDK?

 

HOST PC : UBUNTU18.04, QT5.14.x

YOCTO QT5.15.x

Is there any problem with cross compile and execution?

 

Should I match the QT5 version installed on my HOST PC with the QT5 version of YOCTO?

 

regards!

0 Kudos
Reply
2 Replies

1,146 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kangmw086,

There will be issues when running the version 5.14 since all the files compile and build for 5.15. But you can test your program its not differ too much from version.

 

Regards

 

 

0 Kudos
Reply

1,126 Views
kangmw086
Contributor III

hi

 

So do you mean that I have to install the QT5.15.x version on the HOST PC and cross-compile it?

 

thangs.

0 Kudos
Reply