i.mx6 boardbring up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 boardbring up

5,047 Views
srinivasaporam
Contributor II

Hi,

we are working on i.mx6 customized board which has just come after assembly. we were trying to port OS into it by deploying the SD card image, Uboot etc as explained in the Yocto project.

but when we are powering on the board by putting sd card into the board. nothing is appearing on the monitor which is connected to board through HDMI.

in order to check the correctness and validate our design, we also got evaluation board wandboard quad, for which we have deployed respective image to sd card and powered on the board by putting sd card. then display is coming on the monitor.

So, this has confirmed that we are missing something in our board. while designing the board we taken the references from wand board and as well as sabrelite.

for example, we have taken sd card and other peripheral connections ,schematic and made connections based on wandboard and for some other systems like hdmi, csi we have considered sabrelite reference deisgns.

now, our query is:

Yocto project is specifying procedure deploying the image files to sd card for particular architecture. But,  can we create image files files for customized boards (like our case which is mixture of both wand board and sabrelite). How can we do that.

Labels (5)
0 Kudos
Reply
3 Replies

4,568 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Srinivasa Poram,

Which version BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,568 Views
srinivasaporam
Contributor II

Hi,

we are using 3.10.53 version

0 Kudos
Reply

4,568 Views
igorpadykov
NXP Employee
NXP Employee

HI Srinivasa

please look at attached documents, in particular Yocto Guide

sect.7 Creating a Custom Board Configuration and links

Task #10 - How to create a custom layer

How to add support of custom board into YOCTO - iMX6 Rex Module

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply