i.mx6 GPU with mplayer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 GPU with mplayer

3,956 Views
enricorossi
Contributor I

Dear YuriMuhin_ng,

I would like to resume this thread and ask if NXP now provides GPU support for mplayer on IMX6 platforms.

Thanks for you time.

Best regards,

Enrico

0 Kudos
Reply
4 Replies

3,572 Views
OtavioSalvador
Senior Contributor II

Any reason why to choose mplayer instead of gstreamer?   

0 Kudos
Reply

3,572 Views
enricorossi
Contributor I

Hi OtavioSalvador.

We just have a piece of software built on mplayer and we would like to reuse it. Nothing more.

Thanks for your interest.

Best regards,

Enrico

0 Kudos
Reply

3,572 Views
OtavioSalvador
Senior Contributor II

Oh Ok. I asked because most VPU based apps are being done using GStreamer.   

0 Kudos
Reply

3,572 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The GPU mainly is used for graphic; VPU is intended for playing.

But  section  7.5 (Overlaysink usage) of "i.MX_Linux_User's_Guide.pdf"

describes GPU based overlaysink plugin.

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

i.MX Software|NXP 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------