i.mx6 Deep Sleep Power Connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 Deep Sleep Power Connections

1,069 次查看
dmatthews
Contributor I

We are attempting to implement deep sleep on our custom i.mx6 dual application.  Note that we are not using the PF0100.  Our question is, if NVCC_RGMII and NVCC_ENET are connected to VDDHIGH_CAP, could that cause the weak linear regulator enabled via bit 18 (enable_weak_linreg) of the PMU_REG_2P5n to fail to turn on in DSM (Deep Sleep Mode) or to drop to ~0V?

0 项奖励
回复
1 回复

1,029 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

>if NVCC_RGMII and NVCC_ENET are connected to VDDHIGH_CAP, could that cause the weak linear regulator enabled via >bit 18 (enable_weak_linreg) of the PMU_REG_2P5n to fail to turn on in DSM (Deep Sleep Mode) or to drop to ~0V?

in general yes, behaviour may be unpredictable as VDDHIGH_CAP usage is restricted as described below

pastedImage_1.jpg

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复