i.mx53 voltage setting for LPDDR2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 voltage setting for LPDDR2

ソリューションへジャンプ
2,391件の閲覧回数
KarelH
Contributor II

Helo, I am currently working on loco board with Linux. There is DDR3 which uses voltage 1,5V.

I would like to create own board based on loco, but with LPDDR2, which uses 1,2V. There is MC34708 pmic and it can be set up for both voltages, but I have problem with finding where this voltage is defind in Linux source code.

Could anyone please help me?

Thank you,

Karel

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
2,236件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Karel,

The default voltages of the MC34708 sources are not necessarily defined in Linux code. The MC34708 has 4 pins (PUMS[4:1]) that can be configured to set your desired default voltage configuration. Please see table 11 of the datasheet located in the link below. If you are using SW4 to supply the DDR, then your PUMS[4:1] choice would be 1001 (1 means: tie to VCOREDIG voltage, 0 means: tie to GND). Please check that the rest of the voltages of this option are compliant with your application too. Now, these will be the default power up voltages of the PMIC, but you can change them in your code by writing to the MC34708 registers as soon as you start booting.

Datasheet: http://cache.freescale.com/files/analog/doc/data_sheet/MC34708.pdf?fsrch=1&sr=2

Hope this helps!

Best regards.

Jorge.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,237件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Karel,

The default voltages of the MC34708 sources are not necessarily defined in Linux code. The MC34708 has 4 pins (PUMS[4:1]) that can be configured to set your desired default voltage configuration. Please see table 11 of the datasheet located in the link below. If you are using SW4 to supply the DDR, then your PUMS[4:1] choice would be 1001 (1 means: tie to VCOREDIG voltage, 0 means: tie to GND). Please check that the rest of the voltages of this option are compliant with your application too. Now, these will be the default power up voltages of the PMIC, but you can change them in your code by writing to the MC34708 registers as soon as you start booting.

Datasheet: http://cache.freescale.com/files/analog/doc/data_sheet/MC34708.pdf?fsrch=1&sr=2

Hope this helps!

Best regards.

Jorge.

0 件の賞賛
返信
2,236件の閲覧回数
KarelH
Contributor II

Hi Jorge,

this is exactly what I needed.

Thank you,

Karel

0 件の賞賛
返信