i.mx53 Video preview & record using gstreamer -

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 Video preview & record using gstreamer -

1,522件の閲覧回数
GopiNagaBharath
Contributor IV

Hello,

We are using i.mx53 based system with Linux OS running. We have the USB Camera input which needs to be always shown/previewed on the LCD Display and based on certain conditions, we need to record the video as well in MPEG4 format.

The camera gives the video in VGA resolution with 25fps. We are able to preview the love stream on the LCD, however, we are having the trouble in recording the video with use of gstreamer.

The application is done in Qt and the gstreamer is used for video preview & recording.

Has anybody were able to successfully do the video preview & recording at the same time with the use of gstreamer??

Any help would be appreciated.

Thanks in advance!

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,204件の閲覧回数
BrilliantovKiri
Senior Contributor I

tee

0 件の賞賛
返信