i.mx53 Video preview & record using gstreamer -

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 Video preview & record using gstreamer -

1,491 Views
GopiNagaBharath
Contributor IV

Hello,

We are using i.mx53 based system with Linux OS running. We have the USB Camera input which needs to be always shown/previewed on the LCD Display and based on certain conditions, we need to record the video as well in MPEG4 format.

The camera gives the video in VGA resolution with 25fps. We are able to preview the love stream on the LCD, however, we are having the trouble in recording the video with use of gstreamer.

The application is done in Qt and the gstreamer is used for video preview & recording.

Has anybody were able to successfully do the video preview & recording at the same time with the use of gstreamer??

Any help would be appreciated.

Thanks in advance!

Labels (3)
0 Kudos
Reply
1 Reply

1,173 Views
BrilliantovKiri
Senior Contributor I

tee

0 Kudos
Reply